Access qspi partitions in sd boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Access qspi partitions in sd boot

Jump to solution
1,278 Views
rans
Senior Contributor I

Hello,

I would please like to verify the following,

We are going to use evaluation board (sabre x solo) which has both sd & qspi.

When we Linux boot from sd , do we have access to qspi partitions ?

I guess that if it is decalred in device tree , then linux can see both storage devices, but I am not sure about it, becuase I don't have the source code yet for the evaluation board.

Is it that sd is  /dev/sdX , and qspi as /dev/mtdX ?

On starting working with the board we shall have more idea I'm sure, but as a prepearation, we just wanted to verify the above.

Thank you,

Ran

0 Kudos
Reply
1 Solution
1,155 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ran

it is /dev/mtd, some examples can be found in ucl2.xml from mfg tool.

Linux boot from sd , one has access to qspi partitions.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,156 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ran

it is /dev/mtd, some examples can be found in ucl2.xml from mfg tool.

Linux boot from sd , one has access to qspi partitions.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply