About the meta-fsl-bsp-release layer in freescale-imx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the meta-fsl-bsp-release layer in freescale-imx

Jump to solution
5,101 Views
jasonl
Contributor II

Hello there,

I am trying to include imx layer into our yocto build but unfortunately, the environment is a bit different. The gstreamer1.0_1.8.1.bb file (or more)   in meta-fsl-bsp-release  is hard-coded as FILESEXTRAPATHS_prepend := "${BSPDIR}/sources/poky/meta/recipes-multimedia/gstreamer/files:". But most of the project I have seen they most likely use the path like "~/${DIR}/poky/meta".

Is it possible to change that upstream?

Thanks,

Jason

Tags (2)
1 Solution
2,878 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jason Liu,

The meta-fsl-bsp-release layer is part of the BSP Release, so this layer is not part of the Community BSP wich is part of the Yocto Project (Open Source), that’s why this path is different from other layers.

You can see how the layers are stacked on the following document, it’s not very recent but the basis structure remains.

https://community.nxp.com/docs/DOC-102993

I hope this helps!

Regards,

View solution in original post

1 Reply
2,879 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jason Liu,

The meta-fsl-bsp-release layer is part of the BSP Release, so this layer is not part of the Community BSP wich is part of the Yocto Project (Open Source), that’s why this path is different from other layers.

You can see how the layers are stacked on the following document, it’s not very recent but the basis structure remains.

https://community.nxp.com/docs/DOC-102993

I hope this helps!

Regards,