How to connect a NAND Flash with the i.MX6 microprocessor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to connect a NAND Flash with the i.MX6 microprocessor

1,588 Views
carlosreverbel
Contributor I

Hello,

   I am working on a project to build a custom board for the i.MX6D microprocessor and I would like to use mfgtool to save the bootloader and the O.S. in a NAND Flash chip. The problem is that I cannot find which pins of the microprocessor to connect to the NAND Flash. Could you provide me an schematic showing how to connect the chip to the i.MX6D microprocessor? 

Thank you.

Tags (2)
0 Kudos
Reply
1 Reply

1,407 Views
Yuri
NXP Employee
NXP Employee

Hello,

  please refer to the SABRE for Automotive Infotainment:

https://www.nxp.com/webapp/Download?colCode=SABRE-AI-QUAD-CPU2&Parent_nodeId=1413216565594727840052&... 

https://www.nxp.com/webapp/Download?colCode=SABRE-AI-DUALLITE-CPU2&Parent_nodeId=1413216565594727840... 

SABRE-2|Automotive-Infotainment|i.MX6|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply