About the green line at Video playback on HTML by using WebView on AndroidKK4.4.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the green line at Video playback on HTML by using WebView on AndroidKK4.4.2

3,254 Views
yuuki
Senior Contributor II

Dear all

Our customer plays a video on HTML by using WebView of AndroidKK4.4.2.
However, they have the following problem.

When a Video is switched to next Video, a green line may show in the end of a screen.
This phenomenon occurs very rarely.

Please see an attached video file.
- Issue_02.mp4

They investigate this problem.
Which cord should they refer to?
Could you teach the part they should correct?

May I have advice?


<Environment>
Baord: MX6Q-SABRE-SDB
Display: HDMI output

OS: AndroidKK4.4.2 FSL BSP
Package: AndroidKK4.4.2_Extended Feature Packages(android_kk4.4.2_1.0.0-ga_omxplayer_source)
Patchs: 0001-Fix-the-video-only-stream-can-t-play-issue.patch
             html5_video_issue.patch


Best Regards
Yuuki

Labels (1)
0 Kudos
Reply
7 Replies

2,983 Views
yuuki
Senior Contributor II

Daer all,

Can anyone answer this question?

Please help me.

Best Regards,
Yuuki

0 Kudos
Reply

2,983 Views
yuuki
Senior Contributor II

Daer all,

Our customer has to settle a problem by the end of February.
Does anyone have any information?

Please help me.

Best Regards,
Yuuki

0 Kudos
Reply

2,983 Views
SergioSolis
NXP Employee
NXP Employee

Yuuki,

I cannot reproduce this issue, can you send me the video you are showing and exactly how you reproduce it?

2,983 Views
yuuki
Senior Contributor II

Dear Sergio-san,

I'm sorry to delay.

I requested Video contents from our customer.

They are using application of a subcontracting company.

And they use the contents with which a picture and a video were combined.

Therefore they consider a way.

I consult with them.

Please wait a moment.

Best Regards,

Yuuki

0 Kudos
Reply

2,983 Views
yuuki
Senior Contributor II

Dear Sergio-san,

Thank you very much for your support.

About this problem, local FSL FAE has been contacted to R&D team internally.
Therefore I close this thread.

Best Regards,
Yuuki

0 Kudos
Reply

2,983 Views
SergioSolis
NXP Employee
NXP Employee

Very well then, I will set this thread as 'assume answered'

best regards,

Sergio


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,983 Views
SergioSolis
NXP Employee
NXP Employee

Hello Yuuki,

Our team of experts is reviewing your case and I will update you as soon as I get a response from them.

0 Kudos
Reply