About specifications of the PWM output of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About specifications of the PWM output of i.MX6

Jump to solution
1,062 Views
yuuki
Senior Contributor II

Dear all,

We want to use PWM of i.MX6.
We need the following specifications.

- 9.6KHz +/- 0.5% tolerance
- 104.2usec +/- 0.5% tolerance

Can the PWM output meet these specifications?

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
957 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes PWM output meets these specifications, as

processor clocks are derived from 24MHz and it is quite

accurate, as describes Table 2-20. 24 MHz crystal tolerance guidelines

IMX6DQ6SDLHDG

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
958 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes PWM output meets these specifications, as

processor clocks are derived from 24MHz and it is quite

accurate, as describes Table 2-20. 24 MHz crystal tolerance guidelines

IMX6DQ6SDLHDG

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply