About specifications of the PWM output of i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About specifications of the PWM output of i.MX6

跳至解决方案
1,052 次查看
yuuki
Senior Contributor II

Dear all,

We want to use PWM of i.MX6.
We need the following specifications.

- 9.6KHz +/- 0.5% tolerance
- 104.2usec +/- 0.5% tolerance

Can the PWM output meet these specifications?

Best Regards,
Yuuki

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
947 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes PWM output meets these specifications, as

processor clocks are derived from 24MHz and it is quite

accurate, as describes Table 2-20. 24 MHz crystal tolerance guidelines

IMX6DQ6SDLHDG

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
948 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes PWM output meets these specifications, as

processor clocks are derived from 24MHz and it is quite

accurate, as describes Table 2-20. 24 MHz crystal tolerance guidelines

IMX6DQ6SDLHDG

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复