About preview function in i.MX6SL.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About preview function in i.MX6SL.

ソリューションへジャンプ
35,351件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

Hello. I tested the preview function on MCIMX6SLEVK.

But, the preview didn't function.

Could you tell me the how to preview on MCIMX6SLEVK?

[Board] : MCIMX6SLEVK (LCD: MCIMX28LCD)

[Camera] : OV5642 module

[Image] : L3.10.53_1.0.0 (PreBuild Image)

[gst-launch command line]

$ modprobe ov5642_camera

$ modprobe mxc_v4l2_capture

$ gst-launch-1.0 imxv4l2src device=/dev/video0 ! 'video/x-raw,format=(string)UYVY,width=640,height=480,framerate=(fraction)30/1' ! imxv4l2sink

[Error message]

Can't get caps from capture device, use the default setting.

Perhaps haven't capture device.

====== IMXV4L2SRC: 4.0.2 build on Jan  5 2015 13:31:02. ======

set color key:00010203

====== IMXV4L2SINK: 4.0.2 build on Jan  5 2015 13:31:02. ======

WARNING: erroneous pipeline: could not link imxv4l2src0 to imxv4l2sink0

Best Regards,

Keita

ラベル(3)
1 解決策
31,614件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
31 返答(返信)
7,882件の閲覧回数
norishinozaki
Contributor V

Hi Qiang,

I tried to run mx6s_v4l2_capture.out, but I can't find csi_v4l2_capture.ko in my sdcard.

I configured exactly as you showed us in the last mail.

Here is the all media modules created by bitbake linux-imx -c compile -f && bitbake linux-imx -c deploy.

./media/platform/mxc/capture/ov5640_camera_mipi.ko

./media/platform/mxc/capture/mxc_v4l2_capture.ko

./media/platform/mxc/capture/v4l2-int-device.ko

./media/platform/mxc/capture/ov5640_camera_int.ko

./media/platform/mxc/capture/ipu_fg_overlay_sdc.ko

./media/platform/mxc/capture/adv7180_tvin.ko

./media/platform/mxc/capture/ipu_csi_enc.ko

./media/platform/mxc/capture/ipu_bg_overlay_sdc.ko

./media/platform/mxc/capture/ipu_still.ko

./media/platform/mxc/capture/ipu_prp_enc.ko

./media/platform/mxc/capture/ov5642_camera.ko

./media/platform/mxc/subdev/ov5640_camera.ko

./media/platform/mxc/subdev/mx6s_capture.ko

./media/platform/mxc/subdev/mxc_vadc.ko

./media/platform/mxc/subdev/ov5642_camera.ko

./media/usb/uvc/uvcvideo.ko

./media/usb/gspca/gspca_main.ko

./media/v4l2-core/videobuf2-vmalloc.ko

Do I miss other configurations in kernel?

Attached is my .config and the captures.

Best regards,

Nori Shinozaki

0 件の賞賛
返信
7,882件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

Since you had built in the driver, just run the test command directly: /unit_tests/mx6s_v4l2_capture.out -m 0 -d /dev/video0

The csi_v4l2_capture.ko was replaced by mx6s_capture.ko in 3.14.28 kernel.

7,882件の閲覧回数
norishinozaki
Contributor V

Hello Qiang,

Confirmed working finally.

I didn't need any modules in this configuration.

Now how can I run it with gstreamer?

Customers need it with gstreamer.

Thank you!

Nori Shinozaki

0 件の賞賛
返信
7,882件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

When the camera driver is built in kernel, it is /dev/video0 and the v4l2 output device is the /dev/video1, so the gstreamer test command is:

     gst-launch-1.0 imxv4l2src device=/dev/video0 ! imxv4l2sink device=/dev/video1

For default BSP, it will build camera driver as modules, so v4l2 output device is the /dev/video0, and the camera is /dev/video1, so the test commands are:

$ insmod mx6s_capture.ko

$ insmod ov5642_camera.ko

$ gst-launch-1.0 imxv4l2src device=/dev/video1 ! imxv4l2sink device=/dev/video0

7,891件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

robby​  please continue with the follow up,

0 件の賞賛
返信
7,891件の閲覧回数
robby
NXP Employee
NXP Employee

Hi Karina,


We are now busy with NPI projects and have no resource to support this. Could you please ask AE to support this?

0 件の賞賛
返信
7,891件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Qiang_FSL​ are you able to continue with the follow up here?

0 件の賞賛
返信
7,891件の閲覧回数
keitanagashima
Senior Contributor I

Dear Yuri,

Hello. I added the "csi" parameter in mmcargs.

But, the OV5642 wasn't recognized by i.MX6.

I think that .dtb (.dts) is wrong in L3.14.28 for i.MX6SLEVK.

Please tell me the how to operate the OV5642 in L3.14.28.

We must resolve the issue asap.

Best Regards,

Keita

0 件の賞賛
返信
7,891件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hi,

I forwarded request to the team.

About preview function in i.MX6SL EVK under L3.14.28_1.0.0

Regards,

Yuri

0 件の賞賛
返信
7,891件の閲覧回数
keitanagashima
Senior Contributor I

Hi Yuri,

I tested qt5 image.

My build image and pre-build image didn't operate correctly.

Best Regards,

Keita

0 件の賞賛
返信
7,891件の閲覧回数
keitanagashima
Senior Contributor I

Dear Yuri,

Hello. Thank you for your advice.

I replace the dtb file and i.MX6SL preview was success!

i.MX6SL_Preview.JPG

Best Regards,

Keita

0 件の賞賛
返信