About package installation of glid2 for LTIB of MX6LinuxBSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About package installation of glid2 for LTIB of MX6LinuxBSP

跳至解决方案
2,413 次查看
yuuki
Senior Contributor II

About package installation of glid2 for LTIB of MX6LinuxBSP

Environment is the following.
- MCIMX6DL-SDP
- L3.0.35_4.1.0_ER_SOURCE_BSP

We would like to incorporate gstreamer.


However, the following error occurs.

"import is needed by glib2-2.22.1-1"

Would you teach the method for solving this error?

Beset Regards,

标签 (3)
0 项奖励
回复
1 解答
2,085 次查看
JackLee1z
NXP Employee
NXP Employee

Hi Yuuki,

When I enable glib2 package in ltib configuration > package list, I don't see any issue when I run the build. Can you show me how do you reproduce the problem?

BR,

Jack

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,085 次查看
YixingKong
Senior Contributor IV

Yuuki

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复
2,085 次查看
carl_wei
Contributor I

Hi yuuki, do  you have solved  this error ?  when I build Qt by ltib , the same error occurs:

Processing: glib2

===================

sudo /opt/freescale/ltib/usr/bin/rpm --root /home/Carl/LTIB/ltib/rootfs --dbpath /var/lib/rpm -e --allmatches --nodeps --define '_tmppath /tmp/ltib' glib2 2>/dev/null

sudo /opt/freescale/ltib/usr/bin/rpm --root /home/Carl/LTIB/ltib/rootfs --dbpath /var/lib/rpm --prefix / --ignorearch -ivh --force --excludedocs --define '_tmppath /tmp/ltib' /home/Carl/LTIB/ltib/rpm/RPMS/arm/glib2-2.22.1-1.arm.rpm

error: failed dependencies:

    import   is needed by glib2-2.22.1-1

BSP:

L3.0.35_4.1.0_ER_SOURCE_BSP

2,085 次查看
yuuki
Senior Contributor II

Dear Carl Wei-san,

Thank you for the comment.

This problem has not been solved yet.
I am waiting for the reply from Freescale.

0 项奖励
回复
2,085 次查看
YixingKong
Senior Contributor IV

Yuuki

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复
2,086 次查看
JackLee1z
NXP Employee
NXP Employee

Hi Yuuki,

When I enable glib2 package in ltib configuration > package list, I don't see any issue when I run the build. Can you show me how do you reproduce the problem?

BR,

Jack

0 项奖励
回复