About package installation of glid2 for LTIB of MX6LinuxBSP
Environment is the following.
- MCIMX6DL-SDP
- L3.0.35_4.1.0_ER_SOURCE_BSP
We would like to incorporate gstreamer.
However, the following error occurs. 
"import is needed by glib2-2.22.1-1"
Would you teach the method for solving this error?
Beset Regards,
Solved! Go to Solution.
Hi Yuuki,
When I enable glib2 package in ltib configuration > package list, I don't see any issue when I run the build. Can you show me how do you reproduce the problem?
BR,
Jack
Yuuki
This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.
Thanks,
Yixing
Hi yuuki, do you have solved this error ? when I build Qt by ltib , the same error occurs:
Processing: glib2
===================
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/Carl/LTIB/ltib/rootfs --dbpath /var/lib/rpm -e --allmatches --nodeps --define '_tmppath /tmp/ltib' glib2 2>/dev/null
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/Carl/LTIB/ltib/rootfs --dbpath /var/lib/rpm --prefix / --ignorearch -ivh --force --excludedocs --define '_tmppath /tmp/ltib' /home/Carl/LTIB/ltib/rpm/RPMS/arm/glib2-2.22.1-1.arm.rpm
error: failed dependencies:
import is needed by glib2-2.22.1-1
BSP:
L3.0.35_4.1.0_ER_SOURCE_BSP
Dear Carl Wei-san,
Thank you for the comment.
This problem has not been solved yet. 
I am waiting for the reply from Freescale. 
Yuuki
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
Hi Yuuki,
When I enable glib2 package in ltib configuration > package list, I don't see any issue when I run the build. Can you show me how do you reproduce the problem?
BR,
Jack