About max memory size connected to one CS of EIM of i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About max memory size connected to one CS of EIM of i.MX6

跳至解决方案
1,426 次查看
yuuki
Senior Contributor II

Dear all,

Our customer wants to connect FPGA which has a 256MByte spatial area to one CS of EIM.


According to the reference manual, the following contents are listed.

IMX6DQRM.pdf (Rev2):
22.1.1 Features(P.1007)
"26-bit external address bus, max memory size can be 128 MByte (1 Gigabit)."

However, according to the datasheet, there is 32bit mode.

IMX6DQIEC.pdf (Rev3):
Table 35. EIM Internal Module Multiplexing (P.48)

In this case I think that 256MByte is supported.
2^26 *4 byte =256MByte

Can FPGA of 256MByte spatial area be connected to one CS?

May I have advice?

Best Regards,
Yuuki

标签 (1)
标记 (5)
0 项奖励
回复
1 解答
1,265 次查看
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

answer no, since total address space size is 128 MByte

according to description of ADDRSxx in IOMUXC_GPR1 register.

IMX6DQRM i.MX 6Dual/6Quad Applications Processor Reference Manual.

It also shows memory size allocation per cs.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,266 次查看
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

answer no, since total address space size is 128 MByte

according to description of ADDRSxx in IOMUXC_GPR1 register.

IMX6DQRM i.MX 6Dual/6Quad Applications Processor Reference Manual.

It also shows memory size allocation per cs.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复