About imx8m ddr3l.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About imx8m ddr3l.

2,768 Views
muhualuo
Contributor II

My CPU model is MIMX8MQ5CVAHZAB, and I use DDR3L, the DDR model is mt41k256m16ha-125. Does the CPU of this model support this type of DDR? Is there any reference code?THKS.

Tags (1)
3 Replies

2,588 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Muhua Luo,

Most DDR3L memories compatible with the JEDEC standard are supported by the i.MX8MM. I would recommend reviewing the datasheet and using the programming aid for the i.MX8MM to make sure that it can be setup correctly.

You can find the Programming Aid on the link below. Please look for the i.MX8M Mini DDR3L programming aid on the attachments.

https://community.nxp.com/docs/DOC-340179

I hope this helps!

Regards, 

0 Kudos
Reply

2,585 Views
muhualuo
Contributor II

Hi gusarambula,

Thank you for your reply!

I use MSCALE_DDR_Tool to Calibration my board,when  I  download the DDR scprit, I can get the following output:


*************************************************************************
MX8 DDR Stress Test V2.10
Built on Mar 5 2019 14:26:42
*************************************************************************

--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug

- VMCR Check:
- ttbr0_el3: 0x91d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122

- MMU and cache setup complete

*************************************************************************
ARM clock(CA53) rate: 800MHz
DDR Clock: 800MHz

============================================
DDR configuration
DDR type is DDR3
Data width: 16, bank num: 8
Row size: 15, col size: 10
Two chip selects are used
Number of DDR controllers used on the SoC: 1
Density per chip select: 512MB
Density per controller is: 1024MB
Total density detected on the board is: 1024MB
============================================

MX8M: Cortex-A53 is found

*************************************************************************

I think the tool is recognized my board, but when I click 'Calibration' , there was an error I got, as following:


============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @800Mhz...
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
PMU: Error: dbyte 2 lane 0 failed read deskew
PMU: ***** Assertion Error - terminating *****
[Result] FAILED

What's that meaning? I changged several Regs value, It is the same error output. What should I do next?

The register configuration is in attachment.

thank you.

0 Kudos
Reply

2,585 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Muhua Luo,

Are you still having issues calibrating your DDR? If so would you please share the updated details?

Regards,