About clock tree in i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About clock tree in i.MX6DQ.

跳至解决方案
1,464 次查看
keitanagashima
Senior Contributor I

Dear All,

I referred to ”Figure 18-2. Clock Tree - Part 1” and ”Figure 18-3. Clock Tree - Part 2” in IMX6DQRM(Rev.3).

But, the some difference was seen between jb4.2.2's setting and Reference Manual (RM).

                                                    [RM]   [JB4.2.2]

GPU2D_CORE_CLK_ROOT   352MHz   480MHz

GPU3D_CORE_CLK_ROOT     594MHz   528MHz

GPU3D_SHADER_CLK_ROOT 720MHz   594MHz

ENFC_CLK_ROOT               198MHz   19.8MHz

PERCLK_CLK_ROOT            16.5MHz   22MHz

[Q1]

Why are there differences in the clock?

[Q2]

Is the setting of JB4.2.2 right?

Best Regards,

Keita

标签 (3)
0 项奖励
回复
1 解答
1,272 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Keita,

For MX6DQ, current 2d clock is 480MHz. Current 3d core clock is 528MHz, current 3d shader clock is 594MHz. We don't recommend changing the gpu clock. If any case you want to change it, you can try the clock divider for such root clock. And the clock divider should be done before gpu driver loading. Settings on jb are ok.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,273 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Keita,

For MX6DQ, current 2d clock is 480MHz. Current 3d core clock is 528MHz, current 3d shader clock is 594MHz. We don't recommend changing the gpu clock. If any case you want to change it, you can try the clock divider for such root clock. And the clock divider should be done before gpu driver loading. Settings on jb are ok.

0 项奖励
回复
1,272 次查看
keitanagashima
Senior Contributor I

Dear Alfred,

Hello. Thank you for your reply.

> We don't recommend changing the gpu clock.

OK. I got it.

Best Regards,

Keita

0 项奖励
回复