About clock tree in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About clock tree in i.MX6DQ.

Jump to solution
1,460 Views
keitanagashima
Senior Contributor I

Dear All,

I referred to ”Figure 18-2. Clock Tree - Part 1” and ”Figure 18-3. Clock Tree - Part 2” in IMX6DQRM(Rev.3).

But, the some difference was seen between jb4.2.2's setting and Reference Manual (RM).

                                                    [RM]   [JB4.2.2]

GPU2D_CORE_CLK_ROOT   352MHz   480MHz

GPU3D_CORE_CLK_ROOT     594MHz   528MHz

GPU3D_SHADER_CLK_ROOT 720MHz   594MHz

ENFC_CLK_ROOT               198MHz   19.8MHz

PERCLK_CLK_ROOT            16.5MHz   22MHz

[Q1]

Why are there differences in the clock?

[Q2]

Is the setting of JB4.2.2 right?

Best Regards,

Keita

Labels (3)
0 Kudos
Reply
1 Solution
1,268 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Keita,

For MX6DQ, current 2d clock is 480MHz. Current 3d core clock is 528MHz, current 3d shader clock is 594MHz. We don't recommend changing the gpu clock. If any case you want to change it, you can try the clock divider for such root clock. And the clock divider should be done before gpu driver loading. Settings on jb are ok.

View solution in original post

0 Kudos
Reply
2 Replies
1,269 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Keita,

For MX6DQ, current 2d clock is 480MHz. Current 3d core clock is 528MHz, current 3d shader clock is 594MHz. We don't recommend changing the gpu clock. If any case you want to change it, you can try the clock divider for such root clock. And the clock divider should be done before gpu driver loading. Settings on jb are ok.

0 Kudos
Reply
1,268 Views
keitanagashima
Senior Contributor I

Dear Alfred,

Hello. Thank you for your reply.

> We don't recommend changing the gpu clock.

OK. I got it.

Best Regards,

Keita

0 Kudos
Reply