About clock tree in i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About clock tree in i.MX6DQ.

ソリューションへジャンプ
1,578件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

I referred to ”Figure 18-2. Clock Tree - Part 1” and ”Figure 18-3. Clock Tree - Part 2” in IMX6DQRM(Rev.3).

But, the some difference was seen between jb4.2.2's setting and Reference Manual (RM).

                                                    [RM]   [JB4.2.2]

GPU2D_CORE_CLK_ROOT   352MHz   480MHz

GPU3D_CORE_CLK_ROOT     594MHz   528MHz

GPU3D_SHADER_CLK_ROOT 720MHz   594MHz

ENFC_CLK_ROOT               198MHz   19.8MHz

PERCLK_CLK_ROOT            16.5MHz   22MHz

[Q1]

Why are there differences in the clock?

[Q2]

Is the setting of JB4.2.2 right?

Best Regards,

Keita

ラベル(3)
0 件の賞賛
返信
1 解決策
1,386件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Keita,

For MX6DQ, current 2d clock is 480MHz. Current 3d core clock is 528MHz, current 3d shader clock is 594MHz. We don't recommend changing the gpu clock. If any case you want to change it, you can try the clock divider for such root clock. And the clock divider should be done before gpu driver loading. Settings on jb are ok.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,387件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Keita,

For MX6DQ, current 2d clock is 480MHz. Current 3d core clock is 528MHz, current 3d shader clock is 594MHz. We don't recommend changing the gpu clock. If any case you want to change it, you can try the clock divider for such root clock. And the clock divider should be done before gpu driver loading. Settings on jb are ok.

0 件の賞賛
返信
1,386件の閲覧回数
keitanagashima
Senior Contributor I

Dear Alfred,

Hello. Thank you for your reply.

> We don't recommend changing the gpu clock.

OK. I got it.

Best Regards,

Keita

0 件の賞賛
返信