About a Audio error and application abnormal termination for AndroidKK4.4.2 on i.MX6-SABRE-SDB.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About a Audio error and application abnormal termination for AndroidKK4.4.2 on i.MX6-SABRE-SDB.

4,195件の閲覧回数
yuuki
Senior Contributor II

Our customer is using the following development environment.

<Environment>
Baord: MX6Q-SABRE-SDB
Display: HDMI output

OS: AndroidKK4.4.2 FSL BSP
Package: AndroidKK4.4.2_Extended Feature Packages(android_kk4.4.2_1.0.0-ga_omxplayer_source)
Patchs: 0001-Fix-the-video-only-stream-can-t-play-issue.patch
             html5_video_issue.patch


When a Video playback is repeated, the following error occurs.
And It seems that a Video application is finished forcibly(abnormal termination).

=====Error log=====
I/OMXPlayer( 2291): failed to open file: /data/system/audio_pass_through_pref.
W/linker  ( 2291): lib_aac_dec_v2_arm12_elinux.so has text relocations. This is wasting memory and is a security risk. Please fix.
W/linker  ( 2291): lib_aacplus_dec_v2_arm11_elinux.so has text relocations. This is wasting memory and is a security risk. Please fix.
===================

Are these errors related to abnormal termination?

May I have advice?

Best Regards,
Yuuki

ラベル(1)
0 件の賞賛
返信
14 返答(返信)

3,786件の閲覧回数
yuuki
Senior Contributor II

Daer all,

Can anyone answer this question?

Please help me.

Best Regards,
Yuuki

0 件の賞賛
返信

3,786件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Yuuki,

One question, where did you get the patches you are mentioning?, who provided them to you?

0 件の賞賛
返信

3,786件の閲覧回数
yuuki
Senior Contributor II

Dear Sergio Solis-san,

Thank you for your reply.

I got these patches from FSL.

Best Reagrds,

Yuuki

0 件の賞賛
返信

3,786件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Do you have the requested information Yuuki?

0 件の賞賛
返信

3,786件の閲覧回数
yuuki
Senior Contributor II

Dear Sergio-san,

Thank you for your support.

I am sorry to delay.

Our customer uses the application of the partner.

Therefore I cannot provide the reproduction environment to you.

Would you teach the cause that you can suppose from contents of the error log?

Best Regards,

Yuuki

0 件の賞賛
返信

3,786件の閲覧回数
yuuki
Senior Contributor II

Dear Sergio-san,

Thank you for your support.

May I have any advice for these error logs?

Best Regards,
Yuuki

0 件の賞賛
返信

3,786件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Yuuki,

Is your customer playing an httplive streaming media?  Playing through a web browser or from customer's own application?

thank you,

Sergio

0 件の賞賛
返信

3,786件の閲覧回数
yuuki
Senior Contributor II

Dear Sergio-san,

Thank you for your support.

We are playing the Video contents by using a Web browser based on Chromium.

Best Regards,

Yuuki

0 件の賞賛
返信

3,786件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Can you ask your customer to test this patch?

0 件の賞賛
返信

3,786件の閲覧回数
yuuki
Senior Contributor II

Dear Sergio-san,

We got a log by using this patch.
However, this log includes a confidential information.

Therefore we made a Service Request.

1-3768525447

Would you confirm this SR?

Best Regards,
Yuuki

0 件の賞賛
返信

3,786件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Confirmed, we will continue through the SR.

0 件の賞賛
返信

3,786件の閲覧回数
yuuki
Senior Contributor II

Dear Sergio-san,

Thank you very much for your support.

We confirm it now.

Please give me some time.

Best Regards,

Yuuki

0 件の賞賛
返信

3,786件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Yuuki,

Can you please share more information on how to apply the patches?:

1) baseline, commit hash id

2) whole patches with number 0001-*.patch, 0002-*.patch (i.e. 0001-Fix-* and html5_* which is the first?) . However, at this moment, I tried both sequence but failed to apply the two patches.

3) test files (media files)

4) the test steps.

5) run environment (i.e. boot from sd3 or mmc).

0 件の賞賛
返信

3,786件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Yuuki,

Our Apps team is reviewing your question and I should update you as soon as I get a response from them.

0 件の賞賛
返信