About SSI_CLK_ROOT specification.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About SSI_CLK_ROOT specification.

跳至解决方案
1,550 次查看
takashitakahash
Contributor III

Hi community.

Our customer has below question.

About duty specification of SSI_CLK_ROOT of i.MX6DL.

Please tell us the specifications for Duty of SSI_CLK_ROOT.

If you have any Duty-SPEC, please tell me the Max / Typ/ Min.

标签 (1)
0 项奖励
回复
1 解答
1,485 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Sources of the SSI_CLK_ROOT (PLL4, PLL3) are shown on Figure 18-2 (Clock Tree - Part 1)

of the I.MX6 S/DL RM.   Strictly speaking, jitter, accuracy, duty parameters of internal PLLs are not specified. 
The only specified parameters may be found in the Datasheet(s) in section “PLL’s
Electrical Characteristics”. 
Nevertheless, we can refer to 24 MHz crystal tolerance guidelines of
the Hardware Development Guide, assuming stability (thermal, voltage and other) of PLL output clock is fully defined
by external crystal / oscillator in order to meet USB, PCIe, Ethernet clock specs.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,486 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Sources of the SSI_CLK_ROOT (PLL4, PLL3) are shown on Figure 18-2 (Clock Tree - Part 1)

of the I.MX6 S/DL RM.   Strictly speaking, jitter, accuracy, duty parameters of internal PLLs are not specified. 
The only specified parameters may be found in the Datasheet(s) in section “PLL’s
Electrical Characteristics”. 
Nevertheless, we can refer to 24 MHz crystal tolerance guidelines of
the Hardware Development Guide, assuming stability (thermal, voltage and other) of PLL output clock is fully defined
by external crystal / oscillator in order to meet USB, PCIe, Ethernet clock specs.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复