About ONOFFpin input signal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About ONOFFpin input signal

跳至解决方案
1,782 次查看
goto11
Contributor III

hello,Community

In order to transition to the ON state, when (debounce time) + (ON_TIME) has elapsed, the PMIC_ON_REQ signal will be output high.
If the ONOFFpin low level signal exceeds the debounce time, will it transition to the ON state?
Or do you have to keep ONOFFpin low during the ON_TIME period?

(See attachment)

best regards

Goto

标签 (1)
0 项奖励
回复
1 解答
1,695 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>If the ONOFFpin low level signal exceeds the debounce time, will it transition to the ON state?
>Or do you have to keep ONOFFpin low during the ON_TIME period?

necessary to keep ONOFFpin low during the ON_TIME period.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,696 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>If the ONOFFpin low level signal exceeds the debounce time, will it transition to the ON state?
>Or do you have to keep ONOFFpin low during the ON_TIME period?

necessary to keep ONOFFpin low during the ON_TIME period.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复