About ONOFFpin input signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About ONOFFpin input signal

Jump to solution
1,762 Views
goto11
Contributor III

hello,Community

In order to transition to the ON state, when (debounce time) + (ON_TIME) has elapsed, the PMIC_ON_REQ signal will be output high.
If the ONOFFpin low level signal exceeds the debounce time, will it transition to the ON state?
Or do you have to keep ONOFFpin low during the ON_TIME period?

(See attachment)

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
1,675 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>If the ONOFFpin low level signal exceeds the debounce time, will it transition to the ON state?
>Or do you have to keep ONOFFpin low during the ON_TIME period?

necessary to keep ONOFFpin low during the ON_TIME period.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,676 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>If the ONOFFpin low level signal exceeds the debounce time, will it transition to the ON state?
>Or do you have to keep ONOFFpin low during the ON_TIME period?

necessary to keep ONOFFpin low during the ON_TIME period.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply