About Marking of i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Marking of i.MX6DL

Jump to solution
1,386 Views
yuuki
Senior Contributor II

Dear all,

There was the following marking to the device which we used until now.

    XAC 1522 3N81E TAIW CVACXAG

However, the following is marked to a device delivered this time.

    XAC 1522 3N81E TAIW CVACXY


Would you tell me the difference between "AG" and "Y" of the end?

Best Regards,
Yuuki Murasato

Labels (1)
Tags (3)
1 Solution
1,282 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

    Sorry, but the information you are requesting is treated as confidential info at this time and requires a
signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway.

https://community.nxp.com/docs/DOC-329745  

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

View solution in original post

2 Replies
1,283 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

    Sorry, but the information you are requesting is treated as confidential info at this time and requires a
signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway.

https://community.nxp.com/docs/DOC-329745  

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

1,282 Views
yuuki
Senior Contributor II

Dear Yuri-san

Thank you for your response.
I want to ask NXP support.

Best Reagards,
Yuuki

0 Kudos
Reply