About Marking of i.MX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Marking of i.MX6DL

ソリューションへジャンプ
1,384件の閲覧回数
yuuki
Senior Contributor II

Dear all,

There was the following marking to the device which we used until now.

    XAC 1522 3N81E TAIW CVACXAG

However, the following is marked to a device delivered this time.

    XAC 1522 3N81E TAIW CVACXY


Would you tell me the difference between "AG" and "Y" of the end?

Best Regards,
Yuuki Murasato

ラベル(1)
タグ(3)
1 解決策
1,280件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

    Sorry, but the information you are requesting is treated as confidential info at this time and requires a
signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway.

https://community.nxp.com/docs/DOC-329745  

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,281件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

    Sorry, but the information you are requesting is treated as confidential info at this time and requires a
signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway.

https://community.nxp.com/docs/DOC-329745  

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

1,280件の閲覧回数
yuuki
Senior Contributor II

Dear Yuri-san

Thank you for your response.
I want to ask NXP support.

Best Reagards,
Yuuki

0 件の賞賛
返信