Dear community.
Our customer has question below.
Would you Please advise in the case of about Mig tool of MCIMX 280 DVM 4 B .
※ As soon as possible please respond. As for software writing, when trying to do using Mig tool of NXP , An error message was displayed and writing was impossible.
I think that USB connection between the microcomputer (board) side and the Mig Tool (PC) side has no problem by Mig tool screen display, but when I start by pressing the start button of Mig tool writing, the following error comes out and stops . <error message> "Reason is unknown, failed to run command: type =" boot "body =" Recovery " File = "updater_ivt.sb" timeout = "60" on Error = "" text = "Booting Update Firmware." The semaphore has timed out. " Sorry to trouble you, could you tell me the meaning of the above error and the reasons to be presumed? ※ Error screen and circuit diagram excerpt are attachment .
Thnak you,
Best.
T.Takahashi
解決済! 解決策の投稿を見る。
Hello,
1.
Is the i.MX28 in recovery (USB) boot mode ?
2.
You may try the following approach :
Using Manufacturing Tool for iMX28 in Win7 64-bit
Regards,
Yuri.
Dear Yuri-san.
thank you for your answer.
I received your mail. Thank you very much.
However,I can not download anything from the following drive service, please tell me how to do it.
Https://drive.google.com/file/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx
I can not attach the log file, I will copy the log below.
Wednesday, December 14, 2016 09:47:51
Panel A: Reason is unknown,
Wednesday, December 14, 2016 09:48:15
1 - Panel A Start processing Singlechip NAND <LIST/>.
Panel A Start <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware.".
1 - Panel A DoBoot() - Failed to load updater_ivt.sb to Recovery mode device. (err=1167)
1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware." FAIL code=0x48f.
Panel A: Reason is unknown,failed to run command: type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware." 2 - Panel A Finished processing Singlechip NAND <LIST/> : FAIL code=1167.
Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE
Panel A UtpUpdate Event: DeviceArrival Msg: (null) DevState: Recovery OpState: WAITING_FOR_DEVICE
2 - Panel A Start processing Singlechip NAND <LIST/>.
Panel A Start <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware.".
2 - Panel A Start processing Singlechip NAND <LIST/>.
Panel A Start <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware.".
Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE
2 - Panel A DoBoot() - Failed to load updater_ivt.sb to Recovery mode device. (err=1167)
2 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware." FAIL code=0x48f.
Panel A: Reason is unknown,failed to run command: type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware." 3 - Panel A Finished processing Singlechip NAND <LIST/> : FAIL code=1167.
3 - Panel A DoBoot() - Failed to load updater_ivt.sb to Recovery mode device. (err=1167)
3 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware." FAIL code=0x48f.
Panel A: Reason is unknown,failed to run command: type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware." 4 - Panel A Finished processing Singlechip NAND <LIST/> : FAIL code=1167.
Panel A UtpUpdate Event: DeviceArrival Msg: (null) DevState: Recovery OpState: WAITING_FOR_DEVICE
4 - Panel A Start processing Singlechip NAND <LIST/>.
Panel A Start <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware.".
4 - Panel A Start processing Singlechip NAND <LIST/>.
Panel A Start <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware.".
Panel A: Reason is unknown,4 - Panel A DoBoot() - Failed to load updater_ivt.sb to Recovery mode device. (err=1167)
4 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware." FAIL code=0x48f.
4 - Panel A DoBoot() - Failed to load updater_ivt.sb to Recovery mode device. (err=1167)
4 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware." FAIL code=0x48f.
Hello,
1.
Is the i.MX28 in recovery (USB) boot mode ?
2.
You may try the following approach :
Using Manufacturing Tool for iMX28 in Win7 64-bit
Regards,
Yuri.
Hello
Please check if the i.MX28 is in recovery (USB) boot mode.
Also, I sent You directly the link to load MFG tool working with i.MX28
and supporting USB3 ports on host PC. Please try it.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!