About GPIO input and interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About GPIO input and interrupt

跳至解决方案
1,322 次查看
soichiyamamoto
Contributor V

Hi,

I will ask about i.MX6 Quad.

Can I use the input port and the interrupt function together with the i.MX6 pin?

In the microcomputer used in the past, the terminal using the interrupt function could not be read as a normal input port, so I asked a question.

Best Regards,

soichi/avnet

标签 (1)
0 项奖励
回复
1 解答
1,224 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Soichi

yes one can use the input port and the interrupt function together with the i.MX6 pin.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,225 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Soichi

yes one can use the input port and the interrupt function together with the i.MX6 pin.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复