Please tell me about nand flash boot.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Please tell me about nand flash boot.

1,079件の閲覧回数
shuntarosugawar
Contributor I

I'd like to start U-Boot from NAND Flash (MT29F2G08ABAEAH4), but I'm not going well.
The setting of BOOT_CFG is as follows.
Is the setting incorrect?
Or is it due to the old version of kobs - ng?

The CPU is i.MX6S.


BOOT_MODE0:1
BOOT_MODE1:0

BT_CFG1_0:0
BT_CFG1_1:0
BT_CFG1_2:0
BT_CFG1_3:0
BT_CFG1_4:1
BT_CFG1_5:0
BT_CFG1_6:1
BT_CFG1_7:1

BT_CFG2_0:0
BT_CFG2_1:1
BT_CFG2_2:0
BT_CFG2_3:0
BT_CFG2_4:0
BT_CFG2_5:0
BT_CFG2_6:0
BT_CFG2_7:0

0 件の賞賛
返信
1 返信

935件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi SHUNTARO

for nand boot please check sect.8.5.2 NAND Flash i.MX6SDL Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

For nand programming please use mfg tools and bsp documentation on

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信