About DDR Test Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About DDR Test Tool

Jump to solution
2,000 Views
goto11
Contributor III

Hello,Community

I plan to do LPDDR3 calibration with the DDR Test Tool.
After that, I am planning to conduct a stress test.
The DDR frequency is 533MHz, the maximum frequency of i.MX7D.
Can I set a higher frequency for End Freq?
If so, how many Hz can be set for End Freq?

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
1,887 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Customers can try test their system for frequency range +/-5% of working frequency,

although, strictly speaking, the maximal frequency should not be exceeded.

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
1 Reply
1,888 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Customers can try test their system for frequency range +/-5% of working frequency,

although, strictly speaking, the maximal frequency should not be exceeded.

Regards,

Yuri.

0 Kudos
Reply