About DDR Test Tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About DDR Test Tool

跳至解决方案
2,002 次查看
goto11
Contributor III

Hello,Community

I plan to do LPDDR3 calibration with the DDR Test Tool.
After that, I am planning to conduct a stress test.
The DDR frequency is 533MHz, the maximum frequency of i.MX7D.
Can I set a higher frequency for End Freq?
If so, how many Hz can be set for End Freq?

best regards

Goto

标签 (1)
0 项奖励
回复
1 解答
1,889 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Customers can try test their system for frequency range +/-5% of working frequency,

although, strictly speaking, the maximal frequency should not be exceeded.

Regards,

Yuri.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,890 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Customers can try test their system for frequency range +/-5% of working frequency,

although, strictly speaking, the maximal frequency should not be exceeded.

Regards,

Yuri.

0 项奖励
回复