About DDR Test Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,050件の閲覧回数
goto11
Contributor III

Hello,Community

I plan to do LPDDR3 calibration with the DDR Test Tool.
After that, I am planning to conduct a stress test.
The DDR frequency is 533MHz, the maximum frequency of i.MX7D.
Can I set a higher frequency for End Freq?
If so, how many Hz can be set for End Freq?

best regards

Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,937件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Customers can try test their system for frequency range +/-5% of working frequency,

although, strictly speaking, the maximal frequency should not be exceeded.

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,938件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Customers can try test their system for frequency range +/-5% of working frequency,

although, strictly speaking, the maximal frequency should not be exceeded.

Regards,

Yuri.

0 件の賞賛
返信