APN List is Empty in Android ICS imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

APN List is Empty in Android ICS imx6

Jump to solution
3,409 Views
sanjeevsharma
Contributor IV

Hi All,

While Working on 3G Support in Android ICS In Mobile Network APN List is coming empty and I am not able to set the APN Field's and along with this system doesn't read from apns-conf.xml stored in /system/etc/apns-conf.xml.

Have anyone faced the similar problem ?

Regards

Sanju

Labels (2)
0 Kudos
Reply
1 Solution
2,867 Views
max_tsai
NXP Employee
NXP Employee

hi, You may check the class, "TelephonyProvider.java", which builds the Telephony.db inlcuding "etc/apns-conf.xml".

View solution in original post

0 Kudos
Reply
3 Replies
2,868 Views
max_tsai
NXP Employee
NXP Employee

hi, You may check the class, "TelephonyProvider.java", which builds the Telephony.db inlcuding "etc/apns-conf.xml".

0 Kudos
Reply
2,867 Views
sanjeevsharma
Contributor IV

Hi MaxTSAI,

Now this problem is solved and now i can add entries.I should have hit the back button to save the entries.

Thanks

0 Kudos
Reply
2,867 Views
giorgiosoldavin
Contributor I

Hi,

I have the same problem, and I'm looking to TelephonyProvider.java code but: what have you done for solving it?

Thank you.

Best regards,

Giorgio

0 Kudos
Reply