APN List is Empty in Android ICS imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

APN List is Empty in Android ICS imx6

ソリューションへジャンプ
3,422件の閲覧回数
sanjeevsharma
Contributor IV

Hi All,

While Working on 3G Support in Android ICS In Mobile Network APN List is coming empty and I am not able to set the APN Field's and along with this system doesn't read from apns-conf.xml stored in /system/etc/apns-conf.xml.

Have anyone faced the similar problem ?

Regards

Sanju

ラベル(2)
0 件の賞賛
返信
1 解決策
2,880件の閲覧回数
max_tsai
NXP Employee
NXP Employee

hi, You may check the class, "TelephonyProvider.java", which builds the Telephony.db inlcuding "etc/apns-conf.xml".

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,881件の閲覧回数
max_tsai
NXP Employee
NXP Employee

hi, You may check the class, "TelephonyProvider.java", which builds the Telephony.db inlcuding "etc/apns-conf.xml".

0 件の賞賛
返信
2,880件の閲覧回数
sanjeevsharma
Contributor IV

Hi MaxTSAI,

Now this problem is solved and now i can add entries.I should have hit the back button to save the entries.

Thanks

0 件の賞賛
返信
2,880件の閲覧回数
giorgiosoldavin
Contributor I

Hi,

I have the same problem, and I'm looking to TelephonyProvider.java code but: what have you done for solving it?

Thank you.

Best regards,

Giorgio

0 件の賞賛
返信