ADV7180 bridge driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADV7180 bridge driver

1,857 次查看
amonica
Contributor II

Hi,

  I wanted to make a bridge driver for adv7180 to bind to the subdev driver. I have gone through the V4L2 doc and tried to make a bridge driver to register the adv7180 device driver as a video node in /dev/videoX .

  1.So my doubt first how does the bridge driver and adv7180 communicate?

  2.So have I to insert both if so which one first?

I have added both the code below

 

Regards

Agnes

Original Attachment has been moved to: adv7180.c.zip

Original Attachment has been moved to: bridge2.c.zip

标签 (1)
标记 (2)
1 回复

1,272 次查看
igorpadykov
NXP Employee
NXP Employee

Hi AGNES

please check links below

TVP5150 on IMX6Q

Re: ADV7181 on IMX6Q board

shortly, one needs to use mxc_v4l2_tvin.out to capture video

registered as /dev/video17. Please check example codes of

mxc_v4l2_tvin.out in imx-test package (selected in ltib, below BSP link).

L3.0.35_4.1.0_ER_SOURCE_BSP :

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------