for the DCD header version of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

for the DCD header version of i.MX6

Jump to solution
2,117 Views
yuuki
Senior Contributor II

Dear all,

Would you teach about DCD header version?

I referred to the flash_header.S in Linux BSP.
The version of DCD is 0x40.

"dcd_hdr:          .word 0x40E002D2 /* Tag=0xD2, Len=90*8 + 4 + 4, Ver=0x40 */"


However, in Table 8-31 "DCD Header" of a reference manual, version is 0x41.

"Version: A single byte field set to 0x41"


Do I need to be careful of this difference?

May I have advice?

Best Regards,

Labels (1)
0 Kudos
Reply
1 Solution
1,651 Views
Yuri
NXP Employee
NXP Employee

  Really i.MX6 is one of HAB 4.1, the mentions about ver. 4.0 are derivative

from i.MX53 and do not influence on HAB functionality. One of main differences

between the ver. 4.1 and ver. 4.0 is ability for the rev. 4.1 to support Encrypted

Boot by ROM. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,652 Views
Yuri
NXP Employee
NXP Employee

  Really i.MX6 is one of HAB 4.1, the mentions about ver. 4.0 are derivative

from i.MX53 and do not influence on HAB functionality. One of main differences

between the ver. 4.1 and ver. 4.0 is ability for the rev. 4.1 to support Encrypted

Boot by ROM. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply