8 bit LVDS COMUNICATION AND 1920X720 PROBLEMS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8 bit LVDS COMUNICATION AND 1920X720 PROBLEMS

2,147 Views
dogancanyuksel_
Contributor I

Hi community

I have  problem is my lcd screen has 8 bit lvds communication and 1920x720 but mx6q do not support 1920x720 and has 24 bit LVDS communication? How can i solve this problem ? Could you have any suggestion?

Best regards
dogancan

Labels (2)
Tags (4)
0 Kudos
Reply
1 Reply

1,997 Views
igorpadykov
NXP Employee
NXP Employee

Hi dogancan

24 bit lvds is not supported in nxp bsps and it is necessary to add such support,

may be useful to check:

iMX6QD How to Add 24-bit LVDS Support in Android 

https://community.nxp.com/message/531057?commentID=531057#comment-531057 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply