8 bit LVDS COMUNICATION AND 1920X720 PROBLEMS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

8 bit LVDS COMUNICATION AND 1920X720 PROBLEMS

2,206件の閲覧回数
dogancanyuksel_
Contributor I

Hi community

I have  problem is my lcd screen has 8 bit lvds communication and 1920x720 but mx6q do not support 1920x720 and has 24 bit LVDS communication? How can i solve this problem ? Could you have any suggestion?

Best regards
dogancan

ラベル(2)
タグ(4)
0 件の賞賛
返信
1 返信

2,056件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi dogancan

24 bit lvds is not supported in nxp bsps and it is necessary to add such support,

may be useful to check:

iMX6QD How to Add 24-bit LVDS Support in Android 

https://community.nxp.com/message/531057?commentID=531057#comment-531057 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信