Hi,
I was wondering if NXP has all of the drivers, shared objects, and proprietary firmware necessary to support a 64-bit only build of Android on i.MX8?
I tried building a 64-bit only build of Android 9, but this failed due to the lack of 64-bit drivers for some of the VPU and media components. I didn't have enough time to investigate further.
I would like to know if this is possible, as 32-bit software is something we don't need to support and it would be nice to reduce the amount of legacy code in the system to a minimum. This also helps cut the AOSP build time almost in half, and reduces the size of the OTA update packages.
Thanks,
Max
As i kown, we don't have a plan to publish 64-bit drivers for some of the VPU and media components
Hi,
This helps with porting software and other existing resources to 64-bit, but doesn't help with the missing 64-bit firmware issue.
Has anyone at NXP attempted to build and run Android using build/make/target/product/core_64_bit_only.mk in ProductConfigCommon.mk?
That would be a good starting point for building a 64-bit clean version.
Max