3M touch screen not working if usb plugged in during boot.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

3M touch screen not working if usb plugged in during boot.

跳至解决方案
1,977 次查看
alexanderchung
Contributor II

We have a 3M touch screen on an Android image. The screen connects through HDMI, but the touch controller connects through USB. The problem is that it doesn't recognize any touch events if left plugged in during boot. It only works if we unplug and replug in the usb. Looking under /sys/bus shows that the drivers are bound properly and console shows that it connects during boot.

IMX6 SabreAuto

Android 4.3

Thanks,

Alex

标签 (3)
0 项奖励
回复
1 解答
1,755 次查看
alexanderchung
Contributor II

Turns out I just need to place an Input Device Configuration in /system/usr/idc/

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,756 次查看
alexanderchung
Contributor II

Turns out I just need to place an Input Device Configuration in /system/usr/idc/

0 项奖励
回复
1,755 次查看
CarlosCasillas
NXP Employee
NXP Employee

It is a pleasure to hear that your issue has been solved. Thanks for sharing your solution!

Best regards!

/Carlos

0 项奖励
回复