3M touch screen not working if usb plugged in during boot.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

3M touch screen not working if usb plugged in during boot.

ソリューションへジャンプ
1,985件の閲覧回数
alexanderchung
Contributor II

We have a 3M touch screen on an Android image. The screen connects through HDMI, but the touch controller connects through USB. The problem is that it doesn't recognize any touch events if left plugged in during boot. It only works if we unplug and replug in the usb. Looking under /sys/bus shows that the drivers are bound properly and console shows that it connects during boot.

IMX6 SabreAuto

Android 4.3

Thanks,

Alex

ラベル(3)
0 件の賞賛
返信
1 解決策
1,763件の閲覧回数
alexanderchung
Contributor II

Turns out I just need to place an Input Device Configuration in /system/usr/idc/

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,764件の閲覧回数
alexanderchung
Contributor II

Turns out I just need to place an Input Device Configuration in /system/usr/idc/

0 件の賞賛
返信
1,763件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

It is a pleasure to hear that your issue has been solved. Thanks for sharing your solution!

Best regards!

/Carlos

0 件の賞賛
返信