3M touch screen not working if usb plugged in during boot.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

3M touch screen not working if usb plugged in during boot.

Jump to solution
1,908 Views
alexanderchung
Contributor II

We have a 3M touch screen on an Android image. The screen connects through HDMI, but the touch controller connects through USB. The problem is that it doesn't recognize any touch events if left plugged in during boot. It only works if we unplug and replug in the usb. Looking under /sys/bus shows that the drivers are bound properly and console shows that it connects during boot.

IMX6 SabreAuto

Android 4.3

Thanks,

Alex

Labels (3)
0 Kudos
Reply
1 Solution
1,686 Views
alexanderchung
Contributor II

Turns out I just need to place an Input Device Configuration in /system/usr/idc/

View solution in original post

0 Kudos
Reply
2 Replies
1,687 Views
alexanderchung
Contributor II

Turns out I just need to place an Input Device Configuration in /system/usr/idc/

0 Kudos
Reply
1,686 Views
CarlosCasillas
NXP Employee
NXP Employee

It is a pleasure to hear that your issue has been solved. Thanks for sharing your solution!

Best regards!

/Carlos

0 Kudos
Reply