This patch implements (or exposes) routines to poll the imx uarts. The KGDB drivers need these methods to be implemented or the ttymxc driver is not sufficient. The synthetic CONFIG_CONSOLE_POLL value activates these routines (or CONFIG_SERIAL_MXC_CONSOLE for the polled write). There is still no poll routines in -855-ge067785, which is the September 2010 Linux release from Freescale. Also not in Linux 2.6.36 drivers/serial/imx.c either. $ git diff drivers/serial/mxc_uart.c
diff --git a/drivers/serial/mxc_uart.c b/drivers/serial/mxc_uart.c
index ae6d2e1..728b607 100644
--- a/drivers/serial/mxc_uart.c
+++ b/drivers/serial/mxc_uart.c
@@ -1551,6 +1551,28 @@ mxcuart_pm(struct uart_port *port, unsigned int state, unsigned int oldstate)
clk_enable(umxc->clk);
} +#ifdef CONFIG_CONSOLE_POLL
+/*
+ * Read a character from the UART.
+ */
+static inline int mxcuart_console_read_char(struct uart_port *port)
+{
+ volatile unsigned int status;
+ int ch;
+
+ do {
+ status = readl(port->membase + MXC_UARTUSR2);
+ } while ((status & MXC_UARTUSR2_RDR) == 0);
+ ch = readl(port->membase + MXC_UARTURXD);
+/* Ignore parity errors, etc. */
+/* status = ch | UART_CREAD_BIT; */
+ ch &= 0xff;
+
+ return ch;
+}
+static void mxcuart_console_write_char(struct uart_port *port, char ch);
+#endif
+
/*!
* This structure contains the pointers to the control functions that are
* invoked by the core serial driver to access the UART hardware. The
@@ -1575,14 +1597,18 @@ static struct uart_ops mxc_ops = {
.config_port = mxcuart_config_port,
.verify_port = mxcuart_verify_port,
.send_xchar = mxcuart_send_xchar,
+#ifdef CONFIG_CONSOLE_POLL
+ .poll_put_char = mxcuart_console_write_char,
+ .poll_get_char = mxcuart_console_read_char,
+#endif
};
-#ifdef CONFIG_SERIAL_MXC_CONSOLE
+#if defined(CONFIG_SERIAL_MXC_CONSOLE) || defined (CONFIG_CONSOLE_POLL)
/*
* Write out a character once the UART is ready
*/
-static inline void mxcuart_console_write_char(struct uart_port *port, char ch)
+static void mxcuart_console_write_char(struct uart_port *port, char ch)
{
volatile unsigned int status;
@@ -1592,6 +1618,10 @@ static inline void mxcuart_console_write_char(struct uart_port *port, char ch)
writel(ch, port->membase + MXC_UARTUTXD);
}
+#endif
+
+#ifdef CONFIG_SERIAL_MXC_CONSOLE
+
/*!
* This function is called to write the console messages through the UART port.
*
記事全体を表示