Just sharing some experiences during the development and studying.
Although, it appears some hardwares, it focuses on software to speed up your developing on your hardware.
杂记共享一下在开发和学习过程中的经验。
虽然涉及一些硬件,但其本身关注软件,希望这些能加速您在自己硬件上的开发。
07/25/2024
iMX secondary boot collection
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-secondary-boot-collection/ta-p/19169...
07/25/2024
HSM Code-Signing Journey
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244
25JUL2024 - add pkcs11 proxy
HSM Code-Signing Journey_25JUL2024.pdf
HSM Code-Signing Journey_25JUL2024.txt
06/06/2024
HSM Code-Signing Journey
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244
02/07/2024
Device Tree Standalone Compile under Windows
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Device-Tree-Standalone-Compile-under-Win...
02/07/2024
i.MX8X security overview and AHAB deep dive
i.MX8X security overview and AHAB deep dive - NXP Community
11/23/2023
“Standalone” Compile Device Tree
10/26/2023
Linux Dynamic Debug
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Dynamic-Debug/ta-p/1746611
08/10/2023
u-boot environment preset for sdcard mirror
u-boot environment preset for sdcard mirror - NXP Community
06/06/2023
all(bootloader, device tree, Linux kernel, rootfs) in spi nor demo imx8qxpc0 mek
all(bootloader, device tree, Linux kernel, rootfs)... - NXP Community
09/26/2022
parseIVT - a script to help i.MX6 Code Signing
parseIVT - a script to help i.MX6 Code Signing - NXP Community
Provide run under windows
09/16/2022
create sdcard mirror under windows
create sdcard mirror under windows - NXP Community
08/03/2022
i.MX8MM SDCARD Secondary Boot Demo
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-SDCARD-Secondary-Boot-Demo/ta-p/...
02/16/2022
mx8_ddr_stress_test without UI
12/23/2021
i.MX8 i.MX8X Board Reset
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-i-MX8X-Board-Reset/ta-p/1391130
12/21/2021
regulator userspace-consumer
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/regulator-userspace-consumer/ta-p/138994...
11/24/2021
crypto af_alg blackkey demo
crypto af_alg blackkey demo - NXP Community
09/28/2021
u-boot runtime modify Linux device tree(dtb)
u-boot runtime modify Linux device tree(dtb) - NXP Community
08/17/2021
gpio-poweroff demo
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/gpio-poweroff-demo/ta-p/1324306
08/04/2021
How to use gpio-hog demo
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-gpio-hog-demo/ta-p/1317709
07/14/2021
SWUpdate OTA i.MX8MM EVK / i.MX8QXP MEK
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta...
04/07/2021
i.MX8QXP eMMC Secondary Boot
https://community.nxp.com/t5/i-MX-Community-Articles/i-MX8QXP-eMMC-Secondary-Boot/ba-p/1257704#M45
03/25/2021
sc_misc_board_ioctl to access the M4 partition from A core side
sc_misc_board_ioctl to access the M4 partition fr... - NXP Community
03/17/2021
How to Changei.MX8X MEK+Base Board Linux Debug UART
03/16/2021
How to Change i.MX8MM evk Linux Debug UART
05/06/2020
Linux fw_printenv fw_setenv to access U-Boot's environment variables
Linux fw_printenv fw_setenv to access U-Boot's env... - NXP Community
03/30/2020
i.MX6 DDR calibration/stress for Mass Production
https://community.nxp.com/docs/DOC-346065
03/25/2020
parseIVT - a script to help i.MX6 Code Signing
https://community.nxp.com/docs/DOC-345998
02/17/2020
Start your machine learning journey from tensorflow playground
Start your machine learning journey from tensorflow playground
01/15/2020
How to add iMX8QXP PAD(GPIO) Wakeup
How to add iMX8QXP PAD(GPIO) Wakeup
01/09/2020
Understand iMX8QX Hardware Partitioning By Making M4 Hello world Running Correctly
https://community.nxp.com/docs/DOC-345359
09/29/2019
08/28/2019
eMMC5.0 vs eMMC5.1
https://community.nxp.com/docs/DOC-344265
05/24/2019
How to upgrade Linux Kernel and dtb on eMMC without UUU
How to upgrade Linux Kernel and dtb on eMMC without UUU
04/12/2019
eMMC RPMB Enhance and GP
https://community.nxp.com/docs/DOC-343116
04/04/2019
How to Dump a GPT SDCard Mirror(Android O SDCard Mirror)
https://community.nxp.com/docs/DOC-343079
04/04/2019
i.MX Create Android SDCard Mirror
https://community.nxp.com/docs/DOC-343078
04/02/2019:
i.MX Linux Binary_Demo Files Tips
https://community.nxp.com/docs/DOC-343075
04/02/2019:
Update Set fast boot
eMMC_RPMB_Enhance_and_GP.pdf
02/28/2019:
imx_builder --- standalone build without Yocto
https://community.nxp.com/docs/DOC-342702
08/10/2018:
i.MX6SX M4 MPU Settings For RPMSG update
Update slide CMA Arrangement Consideration
i.MX6SX_M4_MPU_Settings_For_RPMSG_08102018.pdf
07/26/2018
Understand ML With Simplest Code
https://community.nxp.com/docs/DOC-341099
04/23/2018:
i.MX8M Standalone Build
i.MX8M Standalone Build.pdf
04/13/2018:
i.MX6SX M4 MPU Settings For RPMSG update
Add slide CMA Arrangement Consideration
i.MX6SX_M4_MPU_Settings_For_RPMSG_04132018.pdf
09/05/2017:
Update eMMC RPMB, Enhance and GP
eMMC_RPMB_Enhance_and_GP.pdf
09/01/2017:
eMMC RPMB, Enhance and GP
eMMC_RPMB_Enhance_and_GP.pdf
08/30/2017:
Dual LVDS for High Resolution Display(For i.MX6DQ/DLS)
Dual LVDS for High Resolution Display.pdf
08/27/2017:
L3.14.28_Ottbox_Porting_Notes-20150805-2.pdf
MFGTool_Uboot_share_with_NormalRun_sourceCode.pdf
Mass_Production_with_NAND_programmer.pdf
Mass_Production_with_emmc_programmer.pdf
L3.10.53_PianoPI_PortingNote_151102.pdf
AudioCodec_WM8960_Porting_L3.10.53_PianoPI_151012.pdf
TouchScreen_PianoPI_PortingNote_151103.pdf
Accessing_GPIO_From_UserSpace.pdf
https://community.nxp.com/docs/DOC-343344
FreeRTOS for i.MX6SX.pdf
i.MX6SX M4 fastup.pdf
i.MX6_SDCARD_Secondary_Boot_Demo.pdf
i.MX6SX_M4_MPU_Settings_For_RPMSG_10082016.pdf
Security03172017.pdf NOT related to i.MX, only a short memo
Hi Biyong,
Your documents are always helpful, thank you for sharing! I checked the latest "Generate Blob Under Linux" document, but it seems the link doesn't work. Can you please check the link again? Thank you!
Best Regards,
Frank
I don't know about what happened.
I use another way to populate the document.
You can check it can link you to the right place.
And Please let me know it works or not.
Hi Biyong,
It works! Thank you and look forward for your new document.
Best Regards,
Frank
Cool! They are so useful.
Thank you for your sharing!
Looking forward to your update :)
It is useful~
add a link for imx6~