I am using the S32V234 eval board so it's not the same hw than what you are writing about, but just in case you have the answer at hand. On my board, when I try to setup the emmc-rpmb, I get this:
The last one mmc_prep_request(...) if seeing the request as a rpmb request, return BLKPREP_KILL, and the request is dropped, hence the "Operation not permitted" I've seen.
I check the source code of several kernel versions, 4.14 to 3.x, the call is there.
Do you have to do something special to get rpmb access to work, any change to kernel config, or mmc-utils config? Thank you.