i.MX8 i.MX8X Board Reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8 i.MX8X Board Reset

i.MX8 i.MX8X Board Reset

In some cases, such as OTA, need a complete reset/reboot of the i.MX8/i.MX8X.

Current BSP default design for  i.MX8/i.MX8X is partition reset/reboot.

So even using spl bootloader(flash.bin).

The scfw is still running old version.

Not the upgrade version as expected.

Because the reset/reboot by the u-boot or Linux,

Only reset/reboot the A Core partition.

SCU is not reset.

Need to change to the board reset, which will launch entire reset/reboot of the i.MX8/i.MX8X including SCU.

附件
无评分
版本历史
最后更新:
‎01-16-2022 10:22 PM
更新人: