i.MX 8MP MIPI seamless display (连续显示) between U-boot and Kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 8MP MIPI seamless display (连续显示) between U-boot and Kernel

i.MX 8MP MIPI seamless display (连续显示) between U-boot and Kernel

Please notice the following patches are only tested in the environment that is listed below. For the environment with other software versions or hardware equipment, some other editing  may be required

Environment:

  • i.MX 8MP EVK

  • MIPI DSI: MX8-DSI-OLED1 (RM67191)

  • Software: LF5.15.71

U-boot:

1. Apply '0001-Modify-u-boot-to-show-logo-seamlessly.patch' to make sure display related models won't be power off, which will help to achieve seamless display.

Kernel:

1. Apply '0001-Keep-NXP-logo-until-Weston-is-booted-8MP-MIPI.patch' to make sure MIPI-DSI related models won't be re-init in the booting progress.

附件
无评分
版本历史
最后更新:
‎12-09-2024 09:08 AM
更新人: