all(bootloader, device tree, Linux kernel, rootfs) in spi nor demo imx8qxpc0 mek

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

all(bootloader, device tree, Linux kernel, rootfs) in spi nor demo imx8qxpc0 mek

all(bootloader, device tree, Linux kernel, rootfs) in spi nor demo imx8qxpc0 mek

This demo for all(bootloader, device tree, Linux kernel, rootfs) in spi.
It uses raw read(sf read)/raw write(sf write in uuu script) to achieve that.

sf probe 0;
sf read ${fdt_addr} 0x500000 0x100000;
sf read ${loadaddr} 0x600000 0x1E00000;
sf read ${initrd_addr} 0x2400000 0x600000;
setenv bootargs console=${console},${baudrate} earlycon=${earlycon},${baudrate} rdinit=/linuxrc;
booti ${loadaddr} ${initrd_addr} ${fdt_addr}

|-- 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch --- patch for this demo
|-- demo_binary
| |-- flash.b0.bin --- b0 bootloader
| |-- flash.bin --- c0 bootloader
| |-- Image-imx8qxpc0mek.bin --- Linux kernel
| |-- imx8qxp-mek.dtb --- device tree
| |-- uramdisk_boot.rootfs.aarch64.img --- ram disk
| |-- uuu.qspi.all.b0.uuu --- uuu script for b0
| `-- uuu.qspi.all.uuu --- uuu script for c0
`-- readme.txt --- this file


# The spi layout used is:
# - --------- --------------------------------------------
# | | flash.bin | env | dtb | Image |rootfs|
# - --------------- --------------------------------------
# ^ ^ ^ ^ ^ ^ ^
# | | | | | | |
# 0 4kiB 4MiB 5MiB 6MiB 36MiB 42MiB
0x1000 0x400000 0x500000 0x600000 0x2400000

Test:
HW: i.MX8QXP MEK
SW: lf-5.10.72-2.2.0 + 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch

Test log:

SF: Detected mt35xu512aba with page size 256 Bytes, erase size 128 KiB, total 64 MiB
device 0 offset 0x500000, size 0x100000
SF: 1048576 bytes @ 0x500000 Read: OK
device 0 offset 0x600000, size 0x1e00000
SF: 31457280 bytes @ 0x600000 Read: OK
device 0 offset 0x2400000, size 0x600000
SF: 6291456 bytes @ 0x2400000 Read: OK

[ 4.787552] imx6q-pcie 5f010000.pcie: unable to add pcie port.
[ 4.797467] Freeing unused kernel memory: 2944K
[ 4.807379] Run /linuxrc as init process
Starting syslogd: OK
Starting klogd: OK
Running sysctl: OK
Starting network: OK
/bin/sh: can't access tty; job control turned off
/ #

 

Attachments
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----
No ratings
Version history
Last update:
‎06-06-2023 12:02 AM
Updated by: