NOTE: Please suggest bitbake commands you find it useful!
| bitbake command | Description | 
|---|---|
| bitbake <image> | Bake an image (add -k to continue building even errors are found in the tasks execution) | 
| bitbake <package> -c <task> | 
 Example: To (force) compiling a kernel and then build, type: $ bitbake linux-imx -f -c compile $ bitbake linux-imx | 
| bitbake <image > -g -u depexp | Show the package dependency for image. Example: To show all packages included on fsl-image-gui $ bitbake fsl-image-gui -g -u depexp NOTE: This command will open a UI window, so it must be execute on a console inside the host machine (either virtual or native). | 
| bitbake <package> -c devshell | Open a new shell where with neccesary system values already defined for package | 
| hob | bitbake frontend/GUI. | 
| bitbake <package> -c listtasks | List all tasks for package | 
| bitbake virtual/kernel -c menuconfig | Interactive kernel configuration | 
| bitbake <image> -c fetchall | Fetch sources for a particular image | 
| bitbake-layers show-layers | Show layers | 
| bitbake-layers show-recipes "*-image-*" | Show possible images to bake. Without "*-images-*", it shows ALL recipes | 
| bitbake -g <image> && cat pn-depends.dot | grep -v -e '-native' | grep -v digraph | grep -v -e '-image' | awk '{print $1}' | sort | uniq | Show image's packages | 
| bitbake -g <pkg> && cat pn-depends.dot | grep -v -e '-native' | grep -v digraph | grep -v -e '-image' | awk '{print $1}' | sort | uniq | Show package's dependencies | 
| bitbake –v <image> 2>&1 | tee image_build.log | Print (on console) and store verbose baking | 
| bitbake -s | grep <pkg> | Check if certain package is present on current Yocto Setup | 
Yes, it can be used for sure.
Are you getting an error?
In my case, for example, we have:
otavio@nano ~/hacking/ossystems/yocto/build % bitbake-layers show-layers
layer path priority
==========================================================================
meta /home/otavio/hacking/ossystems/yocto/sources/poky/meta 5
meta-yocto /home/otavio/hacking/ossystems/yocto/sources/poky/meta-yocto 5
meta-yocto-bsp /home/otavio/hacking/ossystems/yocto/sources/poky/meta-yocto-bsp 5
meta-oe /home/otavio/hacking/ossystems/yocto/sources/meta-openembedded/meta-oe 1
meta-fsl-arm /home/otavio/hacking/ossystems/yocto/sources/meta-fsl-arm 5
meta-fsl-arm-extra /home/otavio/hacking/ossystems/yocto/sources/meta-fsl-arm-extra 4
meta-fsl-demos /home/otavio/hacking/ossystems/yocto/sources/meta-fsl-demos 4
meta-qt5 /home/otavio/hacking/ossystems/yocto/sources/meta-qt5 7
meta-ossystems /home/otavio/hacking/ossystems/yocto/sources/meta-ossystems 9
meta-ossystems-base /home/otavio/hacking/ossystems/yocto/sources/meta-ossystems-base 8
There is a typo in the penultimate command, it should be "2>&1" instead of "2&>1".
There are even more tasks you can run like: configme, kernel_configcheck, compile_kernelmodules, clean, cleanall, cleansstate etc. I find myself the compile_kernelmodules is very useful for compiling the kernel drivers. You can take the driver and compile outside individually but most of them has lot of dependency, so...
LeonardoSandovalGonzalez bitbake <image> -c fetchall not works for new version yocto, see:FutureMigrationGuide - Yocto Project
-c fetchall is replaced by --runall=fetch
The bitbake -g command changed since yocto 2.3:
BitBake "-g" Output Changes: The package-depends.dot and pn-depends.dot files as previously generated using the bitbake -g command have been removed. A recipe-depends.dot file is now generated as a collapsed version of task-depends.dot instead.