Update
The source code is one week old now, so please, update it!
$ repo sync
Images - the result of a bitbake
Example of a content after bitbake
build_mx6/tmp/deploy/images:
fsl-image-gui-imx6qsabresd-20130505174618.rootfs.ext3
fsl-image-gui-imx6qsabresd-20130505174618.rootfs.sdcard
fsl-image-gui-imx6qsabresd-20130505174618.rootfs.tar.bz2
fsl-image-gui-imx6qsabresd-20130508162511.rootfs.ext3
fsl-image-gui-imx6qsabresd-20130508162511.rootfs.sdcard
fsl-image-gui-imx6qsabresd-20130508162511.rootfs.tar.bz2
fsl-image-gui-imx6qsabresd.ext3
fsl-image-gui-imx6qsabresd.sdcard
fsl-image-gui-imx6qsabresd.tar.bz2
modules-3.0.35-1.1.0+yocto+g0596856-r32.10-imx6qsabresd.tgz
README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt
u-boot.imx
u-boot-imx6qsabresd.imx
u-boot-imx6qsabresd-v2013.04-r3.imx*
uImage
uImage-3.0.35-r32.10-imx6qsabresd-20130505174618.bin
uImage-imx6qsabresd.bin
Get used with generated images. Understand which file is a symbolic link and which one is the image in fact. Symbolic link will always point to latest image.
sdcard image
Take a look how sdcard is generated here meta-fsl-arm - Layer containing Freescale ARM hardware support metadata
The disk layout used is:
0-> IMAGE_ROOTFS_ALIGNMENT reserved to bootloader (not partitioned)
IMAGE_ROOTFS_ALIGNMENT -> BOOT_SPACE kernel and other data
BOOT_SPACE -> SDIMG_SIZE rootfs
Use IMAGE_OVERHEAD_FACTOR to add more space
Please, go to original file in order to understand the disk layout.
It´s basically some initial space for u-boot. One partition for uImage. One partition for rootfs. The total sdcard size will be calculate for every image, if you want to add more empty space inside generated sdcard, use IMAGE_OVERHEAD_FACTOR.
Deploy
Deploy the sdcard image:
$ sudo dd if=fsl-image-gui-imx6qsabresd.sdcard of=/dev/sdX bs=1M
Or, deploy the ext3 rootfs
$ sudo dd if=fsl-image-gui-imx6qsabresd.ext3 of=/dev/sdX2 bs=1M
Or deploy only the tar.bz rootfs
$ sudo mount /dev/sdX2 /mnt/card
$ sudo tar xf imagename-imx53qsb.tar.bz2 -C /mnt/card
In order to deploy only kernel
$ sudo cp uImage-3.0.35-r32.10-imx6qsabresd-20130505174618.bin /media/Boot
In order to deploy only u-boot
$ sudo dd if=u-boot-imx6qsabresd-v2012.10-r3.imx of=/dev/sdX bs=512 seek=2
If using HDMI please, modify u-boot environment arguments:
setenv mmcargs "setenv bootargs console=${console},${baudrate} root=${mmcroot} rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24"
This is the how sdcards are made by meta-fsl-arm. Of course you can use your own. But double check the u-boot bootenv.
Plug your sdcard and let the board boot
To login: root
Go to HOME
Go to Task #3 - The build result
Go to Task#5 - kernel