bitbaked meta-toolchain-qt
Install it with
~/yocto/build/tmp/deploy/sdk$ poky-eglibc-x86_64-arm-toolchain-qt-1.4.1.sh
Download Qtcreator from here http://qt-project.org/downloads
and Install it to Your home directory
edit the bin/qtcreator.sh
source /opt/poky/1.4.1/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi
#! /bin/sh
makeAbsolute() {
case $1 in
/*)
# already absolute, return it
echo "$1"
;;
*)
# relative, prepend $2 made absolute
echo `makeAbsolute "$2" "$PWD"`/"$1" | sed 's,/\.$,,'
;;
esac
}
....
To do it before "#! /bin/sh" is IMPORTANT!!!!
In QtCreator i set
Compiler as
/opt/poky/1.4.1/sysroots/x86_64-pokysdk-linux/usr/bin/armv7a-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++
Qt version as
/opt/poky/1.4.1/sysroots/x86_64-pokysdk-linux/usr/bin/qmake
sysroot as
/opt/poky/1.4.1/sysroots/armv7a-vfp-neon-poky-linux-gnueabi
Put them in a Kit

For connection to Your Board click on Device ---> Manage
Build a new project
and add some to the .pro file

Building the image for Your Board:
add
EXTRA_IMAGE_FEATURES = "debug-tweaks ssh-server-openssh" to Your localconfig
bitbake core-image-sato-sdk
set a password to root via
ssh root@[boardip]
passwd
test connection via
sftp root@[boardip]
start qtcreator
./qtcreator.sh
Message was edited by: Joerg Boge
Good Video to get more Information about Programming are this
Beaglebone: LCD Touchscreen GUI Applications for Embedded Linux - YouTube
Beaglebone: Qt Creator for C++ ARM Embedded Linux Development - YouTube
Beaglebone: Example Qt Embedded Linux Application - YouTube
It is for Beagelbone but for programming Qt it is a good start.
Dieses Dokument wurde aus folgender Diskussion erzeugt: Setup QT Creator with Yocto Build