The Gui-guilder doesn't provide remote debug function in IDE and we still need use Yocto to build project or copy binary to board rootfs.
This knowledge base will provide a solution about how to use VSCode to remote debug LVGL project on i.MX93 EVK board.
Yocto toolchain: L6.6.x
GUI GUILDER: v1.8.0
Need to open GUI GUILDER project in VSCode.
1.Scripts in VScode
1.1 build.sh
Modify build.sh in <LVGL project>/ports/linux
#!/bin/sh
toolchain=$1
if [ -z "$toolchain" ];then
toolchain=/opt/fsl-imx-xwayland/6.1-mickledore/sysroots/x86_64-pokysdk-linux/usr/share/cmake/armv8a-poky-linux-toolchain.cmake
if [ ! -r $toolchain ];then
toolchain=/opt/fsl-imx-xwayland/6.1-langdale/sysroots/x86_64-pokysdk-linux/usr/share/cmake/armv8a-poky-linux-toolchain.cmake
fi
fi
toolchain_path=$(echo $toolchain |sed -E 's,^(.*)/sysroots/.*,\1,')
toolchain_arch=armv8a-poky-linux
if [ ! -r $toolchain -o ! -r "$toolchain_path/environment-setup-$toolchain_arch" ];then
echo "ERROR: Yocto Toolchain not installed?"
exit 1
fi
if [ -n "$BASH_SOURCE" ]; then
ROOTDIR="`readlink -f $BASH_SOURCE | xargs dirname`"
elif [ -n "$ZSH_NAME" ]; then
ROOTDIR="`readlink -f $0 | xargs dirname`"
else
ROOTDIR="`readlink -f $PWD | xargs dirname`"
fi
BUILDDIR=$ROOTDIR/../build
rm -fr $BUILDDIR
mkdir $BUILDDIR
. "$toolchain_path/environment-setup-$toolchain_arch"
echo "start build..."
cd $ROOTDIR/linux/lv_drivers/wayland/
cmake .
make
cd $BUILDDIR
toolchain_path=/opt/fsl-imx-wayland/6.6-scarthgap/sysroots/x86_64-pokysdk-linux/usr/share/cmake/armv8a-poky-linux-toolchain.cmake
cmake -G 'Ninja' .. -DCMAKE_TOOLCHAIN_FILE=$toolchain_path -Wno-dev -DLV_CONF_BUILD_DISABLE_EXAMPLES=1 -DLV_CONF_BUILD_DISABLE_DEMOS=1 -DCMAKE_CXX_FLAGS="-ggd3 -O0" -DCMAKE_BUILD_TYPE=Debug
ninja
if [ -e gui_guider ];then
echo "Binary locates at $(readlink -f gui_guider)"
ls -lh gui_guider
fi
# Copy binary to board
scp $BUILDDIR/gui_guider root@192.168.31.243:/opt
1.2 tasks.json
{
"version": "2.0.0",
"tasks": [
{
"label": "Build",
"type": "shell",
"command": "./build.sh /opt/fsl-imx-wayland/6.6-scarthgap",
"options": {
"cwd": "${workspaceFolder}/ports/linux"
},
"problemMatcher": [
"$gcc"
],
}
]
}
1.3 launch.json
miDebuggerServerAddress is board ip address.
{
"version": "0.2.0",
"configurations": [
{
"name": "(gdb) Launch",
"preLaunchTask": "Build",
"type": "cppdbg",
"request": "launch",
"program": "${workspaceFolder}/build/gui_guider",
"args": [],
"stopAtEntry": false,
"cwd": "${workspaceFolder}/",
"environment": [],
"externalConsole": false,
"MIMode": "gdb",
"logging": {
"engineLogging": true,
"trace": true,
"traceResponse": true
},
"debugStdLib":true,
"miDebuggerPath":"/usr/bin/gdb-multiarch", //DO NOT USE GDB IN SDK!!!!
"miDebuggerServerAddress": "192.168.31.243:12345",
"setupCommands": [
{
"description": "Enable pretty-printing for gdb",
"text": "-enable-pretty-printing",
"ignoreFailures": true,
"text": "set remotetimeout 100",
}
]
}]
}
2. Launch gdbserver on board
export SHELL=/opt/gui_guider
gdbserver 192.168.31.243:12345 /opt/gui_guider
3. Debug in VSCode
Click (gdb)launch, the source code will be compiled.

Then you will see the breakpoint in program.

Enjoy your debug~