How to run an SquareLine project on i.MX 93 EVK using FrameBuffer.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to run an SquareLine project on i.MX 93 EVK using FrameBuffer.

How to run an SquareLine project on i.MX 93 EVK using FrameBuffer.

Introduction

LVGL is a graphics library to run on devices using a limited amount of resources.

Previously, we have ran an LVGL demo from the LVGL repository, this contains a couple more demos which all of them are pieces of code included and lends us the opportunity to evaluate the library in a quick and easy way.

GUI projects are developed by customers through a lot more options than bare code, there are GUI tools that translate a graphic asset into LVGL code, in this demonstration we will use a tool that's widely used in MCU GUI development and translate the GUI created into LVGL code; SquareLine.

NOTE: refer to the appendix for precedent LVGL documents on i.MX series processors.

HW set-up

  • i.MX 93 EVK boot over eMMC/uSD to Linux Factory or Ubuntu.
  • Connect power and debug receptables.
  • Connect MX8_DSI_OLED1 to J701 (MIPI DSI) through MiniSAS cable.

SquareLine set-up

Download the latest version of SquareLine under the following link according to your host system.

JosephAtNXP_0-1732571954892.png

NOTE: This document is intended for demonstration of templates included within the tool, so it's recommended to download a free trial, for formal development please refer to the appendix of this document.

Unzip and execute the installer, this is the windows prompt.

JosephAtNXP_1-1732571954893.png

 

Demo download

After setting SquareLine up go to the example section, we will demonstrate the thermostat capabilities with the Thermostat Demo.

JosephAtNXP_2-1732571954894.png

We can directly export these UI files and they would be graphically ready to be build, click on Export -> Export UI Files and select your preferred destination to save these.

JosephAtNXP_3-1732571954894.png

 

LVGL setup. Option 1 Fresh Environment

Clone LVGL and LV_DRIVERS repositories, this is a .gitmodules file that points to the specific branches needed.

[submodule "lvgl"]
path = lvgl
url = https://github.com/lvgl/lvgl.git
branch = release/v8.3
[submodule "lv_drivers"]
path = lv_drivers
url = https://github.com/lvgl/lv_drivers.git
branch = release/v8.3

NOTE: If you are using other methods, you should point to these commits, lv_drivers @ 8cdabe8 and lvgl @ f2c1032.

Gather the necessary files described below from the LVGL Linux Port example found here.

  • Makefile
  • lv_conf.h
  • lv_drv_conf.h
  • main.c
  • mouse_cursor_icon.c

Patch the Makefile.

+ include $(LVGL_DIR)/thermostat/thermostat.mk

Patch the lv_drv_conf.h

#  define EVDEV_NAME   "/dev/input/event10"        /*You can use the "evtest" Linux tool to get the list of devices and test them*/
+#  define EVDEV_NAME   "/dev/input/event<Number>"

NOTE: This changes according to the output of # evtest.

Patch lv_conf.h

-#define LV_FONT_MONTSERRAT_20 0
+#define LV_FONT_MONTSERRAT_20 1

Patch the main.c

-    disp_drv.hor_res    = 800;
-    disp_drv.ver_res    = 480;
+    disp_drv.hor_res    = 1080;
+    disp_drv.ver_res    = 1920;
…
-    /*Create a Demo*/
-    lv_demo_widgets();
+    /*Create a Squareline Demo*/
+    ui_init();

LVGL Setup. Option 2 with LVGL demos already running

Gather the necessary files described below from the LVGL Linux Port example found here.

  • Makefile
  • lv_conf.h
  • lv_drv_conf.h
  • main.c
  • mouse_cursor_icon.c

Patch the lv_drv_conf.h

#  define EVDEV_NAME   "/dev/input/event10"        /*You can use the "evtest" Linux tool to get the list of devices and test them*/
+#  define EVDEV_NAME   "/dev/input/event<Number>"

NOTE: This changes according to the output of # evtest.

Patch the main.c

-    disp_drv.hor_res    = 800;
-    disp_drv.ver_res    = 480;
+    disp_drv.hor_res    = 1080;
+    disp_drv.ver_res    = 1920;
…
-    /*Create a Demo*/
-    lv_demo_widgets();
+    /*Create a Squareline Demo*/
+    ui_init();

Run the demo

Build the demo with the following command and copy the ./demo output to the i.MX 93 EVK RootFS.

# source /opt/path/to/your/toolchain
# make clean
# make

The demo can be ran with the following commands.

# systemctl stop weston # For LF
$ sudo service gdm3 stop # For Ubuntu

# ./demo
JosephAtNXP_4-1732572830444.jpeg

 

Conclusion

SquareLine demos can run in prebuilt and basic builds of i.MX processors through FB, which can enable a quick set-up for GUI testing before moving to use a windowing stack without sacrificing any features.

Appendix

Document: How to run LGVL on iMX using framebuffer

Official page for pricing information

无评分
版本历史
最后更新:
‎11-25-2024 03:25 PM
更新人: