How to reduce the CPU Frequency on iMX8M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to reduce the CPU Frequency on iMX8M

How to reduce the CPU Frequency on iMX8M

 

For some applications, we need to reduce the CPU Frequency, but if you are not familiar with our BSP or our devices probably you need some help to do some configurations.

 

In this post, I will share the configuration to set up lower frequencies (100MHz, 200MHz, 400Mhz, 600MHz, 800MHz, and 1000MHz) on iMX8MP, iMX8MN, and iMX8MM.

 

Note: Works on Kernel 6.1.xx (not tested on oldest BSP)

 

1- We have to modify the PLL driver to set the proper parameters to lower frequencies.

The file to modify is "clk-pll14xx.c" adding the following lines:

 

https://github.com/nxp-imx/linux-imx/blob/770c5fe2c1d1529fae21b7043911cd50c6cf087e/drivers/clk/imx/c...

 

static const struct imx_pll14xx_rate_table imx_pll1416x_tbl[] = {

        PLL_1416X_RATE(1800000000U, 225, 3, 0),

        PLL_1416X_RATE(1600000000U, 200, 3, 0),

        PLL_1416X_RATE(1500000000U, 375, 3, 1),

        PLL_1416X_RATE(1400000000U, 350, 3, 1),

        PLL_1416X_RATE(1200000000U, 300, 3, 1),

        PLL_1416X_RATE(1000000000U, 250, 3, 1),

        PLL_1416X_RATE(800000000U, 200, 3, 1),

        PLL_1416X_RATE(750000000U, 250, 2, 2),

        PLL_1416X_RATE(700000000U, 350, 3, 2),

        PLL_1416X_RATE(600000000U, 300, 3, 2),

+ PLL_1416X_RATE(400000000U, 200, 3, 2),

+ PLL_1416X_RATE(200000000U, 200, 3, 3),

+ PLL_1416X_RATE(100000000U, 200, 3, 4),

};

 

2- Once the pll driver has been modified, only we have to add the values on the opp-table according to the device that you will use.

 

2.1- For iMX 8MP:

 

https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp.dtsi

 

     

 a53_opp_table: opp-table {

                compatible = "operating-points-v2";

                opp-shared;

 

+ opp-100000000 {

+ opp-hz = /bits/ 64 <100000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0x8a0>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

+ opp-200000000 {

+ opp-hz = /bits/ 64 <200000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0x8a0>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

+ opp-400000000 {

+ opp-hz = /bits/ 64 <400000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0x8a0>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

+ opp-600000000 {

+ opp-hz = /bits/ 64 <600000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0x8a0>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

+ opp-800000000 {

+ opp-hz = /bits/ 64 <800000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0x8a0>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

+ opp-1000000000 {

+ opp-hz = /bits/ 64 <1000000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0x8a0>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

                opp-1200000000 {

                        opp-hz = /bits/ 64 <1200000000>;

 

2.2 For iMX8MM:

 

https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mm.dtsi

 

 

      a53_opp_table:

                opp-table {

                compatible = "operating-points-v2";

                opp-shared;

 

+ opp-100000000 {

+ opp-hz = /bits/ 64 <100000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0xe>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

+ opp-200000000 {

+ opp-hz = /bits/ 64 <200000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0xe>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

+ opp-400000000 {

+ opp-hz = /bits/ 64 <400000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0xe>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

+ opp-600000000 {

+ opp-hz = /bits/ 64 <600000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0xe>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

+ opp-800000000 {

+ opp-hz = /bits/ 64 <800000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0xe>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

+ opp-1000000000 {

+ opp-hz = /bits/ 64 <1000000000>;

+ opp-microvolt = <850000>;

+ opp-supported-hw = <0xe>, <0x7>;

+ clock-latency-ns = <150000>;

+ opp-suspend;

+ };

 

                opp-1200000000 {

                        opp-hz = /bits/ 64 <1200000000>;

 

2.3- For iMX8MN:

 

https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mn.dtsi

 

compatible = "operating-points-v2";
 		opp-shared;
 
+                opp-100000000 {
+                        opp-hz = /bits/ 64 <100000000>;
+                        opp-microvolt = <850000>;
+                        opp-supported-hw = <0xb00>, <0x7>;
+                        clock-latency-ns = <150000>;
+                        opp-suspend;
+                };
+
+                opp-200000000 {
+                        opp-hz = /bits/ 64 <200000000>;
+                        opp-microvolt = <850000>;
+                        opp-supported-hw = <0xb00>, <0x7>;
+                        clock-latency-ns = <150000>;
+                        opp-suspend;
+                };
+
+                opp-400000000 {
+                        opp-hz = /bits/ 64 <400000000>;
+                        opp-microvolt = <850000>;
+                        opp-supported-hw = <0xb00>, <0x7>;
+                        clock-latency-ns = <150000>;
+                        opp-suspend;
+                };
+
+                opp-600000000 {
+                        opp-hz = /bits/ 64 <600000000>;
+                        opp-microvolt = <850000>;
+                        opp-supported-hw = <0xb00>, <0x7>;
+                        clock-latency-ns = <150000>;
+                        opp-suspend;
+                };
+
+                opp-800000000 {
+                        opp-hz = /bits/ 64 <800000000>;
+                        opp-microvolt = <850000>;
+                        opp-supported-hw = <0xb00>, <0x7>;
+                        clock-latency-ns = <150000>;
+                        opp-suspend;
+                };
+
+                opp-1000000000 {
+                        opp-hz = /bits/ 64 <1000000000>;
+                        opp-microvolt = <850000>;
+                        opp-supported-hw = <0xb00>, <0x7>;
+                        clock-latency-ns = <150000>;
+                        opp-suspend;
+                };
+
 		opp-1200000000 {
 			opp-hz = /bits/ 64 <1200000000>;
 			opp-microvolt = <850000>;

 

After that, you should note the changes under Linux.

 

These commands return information about the system and the current settings.

 

• The kernel is pre-configured to support only certain frequencies. The list of frequencies currently supported

can be obtained from:

cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_frequencies

 

• To get the available scaling governors:

cat /sys/devices/system/cpu/*/cpufreq/scaling_available_governors

 

• To check the current CPU frequency:

cat /sys/devices/system/cpu/*/cpufreq/cpuinfo_cur_freq

 

The frequency is displayed depending on the governor set.

 

• To check the maximum frequency:

cat /sys/devices/system/cpu/*/cpufreq/cpuinfo_max_freq

 

• To check the minimum frequency:

cat /sys/devices/system/cpu/*/cpufreq/cpuinfo_min_freq

 

These commands set a constant CPU frequency:

 

• Use the maximum frequency:

echo performance > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor

 

• Use the current frequency to be the constant frequency:

echo userspace > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor

 

• The following two commands set the scaling governor to a specified frequency, if that frequency is supported.

 

If the frequency is not supported, the closest supported frequency is used:

 

echo userspace > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
echo <frequency> > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed

 

Chavira_0-1708555234422.png

 

ラベル(2)
添付
コメント

This is really useful & helpful information.

I used a similar method to enable 800 MHz, 1 GHz and 1.5 GHz on an IMX8M CPU.

When running on different frequencies did you notice the power consumption change? I'm not seeing any change.

 

50%が役に立ったと言っています (2/4)
バージョン履歴
最終更新日:
‎02-22-2024 11:24 AM
更新者: