HDMI Dongle Reference Design Release

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI Dongle Reference Design Release

HDMI Dongle Reference Design Release

HDMI Dongle SW:


The attachment is an HDMI dongle patch based on R13.4 GA. The patches include r13.4-ga-add-on-patches. You can patch it after applying R13.4 GA patch such as add-on patches. You can run script to revb_dongle_patch_install.sh to apply these patches.

How to apply the hdmidongle_REVB_R13.4_patch-20121115.tgz:

1. Suppose your android source top is ~/myandroid

2. tar zfvx hdmidongle_REVB_R13.4_patch-20121115.tgz -C ~/

3. copy revb_dongle_patch_install.sh to ~/

4. cd hdmidongle_REVB_R13.4_patch

5. ~/revb_dongle_patch_install.sh

6. The  revb_dongle_patch_install.sh will take ~/myandroid as default directory to do patch

7. If your android source tree top is not ~/myandroid. For example, ~/myandroid_ICS, please run ~/revb_dongle_patch_install.sh ~/myandroid_ICS

 

The following is the release notes for  hdmidongle_REVB_R13.4_patch-20130118.tgz


1. New features:
   a. uboot fastboot
   b. ldo bypass
   c. ntfs support

   d. bluetooth A2DP

 

2. Bug fix
   a. WifiDirect connect issue
   b. realtek throughput issue with TPLink AP

 

3. File list:

   README.TXT                                      --- this file
   0001-uboot_fastboot.patch                       --- uboot fastboot  patch
   0002-LDOBYPASS.patch                            --- enable ldo bypass  patch
   0003-WifiDirect.patch                           --- wifi direct connect patch
   0004-ntfs_support.patch                         --- ntfs support patch
   0005-BT_enable.patch                            --- enable bluetooth A2DP
   0006-1G_boot_stable.patch                       --- make 1G bootup stable
   ntfs-3g.tar.gz                                  --- open source ntfs-3g for ntfs support
   rtl8192ce_v4.0.0_6239.20121226_TPIOT1.tgz       --- realtek new driver for TPLink AP throughput issue
   MD5SUM.TXT                                      --- md5 check sum

 

4. Patch guide
   Please run md5sum -c MD5SUM.TXT first to confirm all the files received are ok.
   All these patches are based on the patch release hdmidongle_REVB_R13.4_patch-20121115.tgz
   You need to do as following: R13.4 GA--->patch hdmidongle_REVB_R13.4_patch-20121115.tgz --> patch hdmidongle_REVB_R13.4_patch-20130118.tgz
   Supposed the ~/myandroid is your top directory of the android source tree.
   Please run the following command to apply the patches .
   $tar zfvx hdmidongle_REVB_R13.4_patch-20130118.tgz -C ~/
   $cd ~/myandroid
   $git apply  ~/hdmidongle_REVB_R13.4_patch-20130118/0001-uboot_fastboot.patch --verbose
   $git apply  ~/hdmidongle_REVB_R13.4_patch-20130118/0002-LDOBYPASS.patch --verbose
   $git apply  ~/hdmidongle_REVB_R13.4_patch-20130118/0003-WifiDirect.patch --verbose
   $git apply  ~/hdmidongle_REVB_R13.4_patch-20130118/0004-ntfs_support.patch --verbose
   $git apply  ~/hdmidongle_REVB_R13.4_patch-20130118/0005-BT_enable.patch --verbose
   $git apply  ~/hdmidongle_REVB_R13.4_patch-20130118/0006-1G_boot_stable.patch --verbose
   $rm -rf kernel_imx/drivers/net/wireless/rtl8192ce
   $tar zfvx ~/hdmidongle_REVB_R13.4_patch-20130118/rtl8192ce_v4.0.0_6239.20121226_TPIOT1.tgz
   $tar zfvx ~/hdmidongle_REVB_R13.4_patch-20130118/ntfs-3g.tar.gz -C external

 

5. Build and run

 

 

new patch 0007-battery_always_full.patch:

 

Some games check the battery capacity to determine, it could run or not. But on the hdmi dongle we have no real battery, it makes some games can not run on the hdmi dongle.  We enable the fake battery let the andorid feel it has battery and it is 100% full.

1. Please use this patch after patch hdmidongle_REVB_R13.4_patch-20130118.tgz

2. suppose your android top directory is ~/myandroid and you put he 0007-battery_always_full.patch in your home directory ~

3. cd ~/myandroid

4. git apply --verbose ~/0007-battery_always_full.patch

5. please rebuild bootimage and run

 

patch   0008-boot_unlock_screen.patch:

When bootup, it goes into desktop rather than screen locker.

 

1. suppose your android top directory is ~/myandroid and you put the 0008-boot_unlock_screen.patch in your home directory ~

2. cd ~/myandroid

3. git apply --verbose ~/0008-boot_unlock_screen.patch

4. please rebuild systemtimage and run

2. cd ~/myandroid

3. git apply --verbose ~/0008-boot_unlock_screen.patch


patch 0009-uboot-enable-mmu-fix.patch:

This patch is for some issue in mmu enable.

It will improve all the modules in uboot.

 

1. suppose your android top directory is ~/myandroid and you put the 0009-uboot-enable-mmu-fix.patch in your home directory ~

2. cd ~/myandroid

3. git apply --verbose ~/0009-uboot-enable-mmu-fix.patch

4. please rebuild uboot  and rub

 

 

patch tarball   hdmidongle_REVB_R13.4_patch-20130123.tgz:

 

hdmidongle_REVB_R13.4_patch-20130123.tgz contains 0007-battery_always_full.patch  0008-boot_unlock_screen.patch 0009-uboot-enable-mmu-fix.patch

remove attached files here: 0007-battery_always_full.patch  0008-boot_unlock_screen.patch 0009-uboot-enable-mmu-fix.patch

 

 

Remove hdmidongle_REVB_R13.4_patch-20130123.tgz, hdmidongle_REVB_R13.4_patch-20130118.tgz and upload hdmidongle_REVB_R13.4_patch-20130124.tgz

 

hdmidongle_REVB_R13.4_patch-20130124.tgz  contains all patches in hdmidongle_REVB_R13.4_patch-20130123.tgz, hdmidongle_REVB_R13.4_patch-20130118.tgz.

Please use the  hdmidongle_REVB_R13.4_patch-20130124.tgz.

 

hdmidongle_REVB_R13.4_patch-20130131.tgz:

Besides all the patches released before.

Three more patches are added in this patch tar ball.

 

 

0010-boot_disable_screenlocker.patch                     --- For fix  0008-boot_unlock_screen.patch

0011-wm8326-DC_CONTROL_RATE.patch                        --- Change the wm8326 pmic rate to immediate voltage change

0012-Added-default-video-mode-check-make-sur.patch       --- Video mode check

 

hdmidongle_REVB_R13.4_patch-20130201.tgz:

 

Just change the readme  to place emphasis on   the 0006-1G_boot_stable.patch reverse

 

Reverse patch 0008-boot_unlock_screen.patch and 0006-1G_boot_stable.patch

 

0008-boot_unlock_screen.patch: it has some problem but doesn't do any harm to the hdmi dongle.

                                                 Please use 0010-boot_disable_screenlocker.patch, instead.

0006-1G_boot_stable.patch:  The patch take more cpu delay to adapt the pmic, we change the pmic setting

                                            in  0010-boot_disable_screenlocker.patch. This patch is no needed. And it will lower

                                           the performance. Please reverse it.

                                           cd ~/myandroid

                                           git apply --verbose ~/0006-1G_boot_stable.patch                                          

                                             

 

hdmidongle_REVB_R13.4_patch-20130221.tgz:

There are three important fixes include in this release. They make the dongle stable.

1. lowmem killer issue fix

2. Update realtek wifi driver to fix the soft ap issue

3. Wifi p2p framework fix to resovle wifi direct only one side work issue

 

Please read the README.TXT for detail and the other changes.

 

hdmidongle_REVB_R13.4_patch-20130308.tgz:

This patch tar ball include all the patches in hdmidongle_REVB_R13.4_patch-20130221.tgz.

Besides, it has a new patches 0020-DL_WifiDirect_Concunrrent_crash_fix.patch to fix the crash issue on DL board.

 

HDMI Dongle HW:

 

HDMI Dongle schematic, pcb, gerber and BOM have been attached, the detailed hardware feature has been list below:

 

Android 4.x HDMI Dongle SPECIFICATION
Core Configure
Operating SystemAndroid 4.x Operating System Based on Micro-PC Platform
CPU ProcessorFreescale i.MX6x DualLite/Quad Core
DRAM StorageDDR3 1GigaByte Size, Data rate 1066MT/s
Flash Storage4GigaByte NAND flash ROM
Power System
Power SupplyDC JACK / Micro USB : 5V/2A
LED StatusGreen: Power ON; Red: System Run
Socket/Connector
MicroSD SocketSDXC Support, Up to 32GB size
USB HOST 2.0USB 2.0 HOST Support
USB OTG 2.0USB 2.0 OTG Support
Display/Audio
HDMI OutputHDMI TypeA Plug connector, 1080p@60Hz output
Video DecoderSupport Variety of Video Format: MPEG4/H.263/H.264/MJPEG/Xvid/VC-1/WMV/MPEG2/VP8...
Audio DecoderSupport Variety of Audio Format: MP3/AAC/LPCM/FLAC/AMR/AC3/WMA/Vorbis
GPU SupportGC2000 GPU core,2D/3D engine support,OpenGL support
Wireless Network
WiFi NetworkIEEE 802.11b/g/n,Up to 300Mbps,AP/P2P/Sta Mode Support
Others
KeyRecovery key support
RevB2

 

3620_3620.jpgIMG1080.jpg

3621_3621.jpgIMG1335.jpg

3624_3624.jpgIMG1138.jpg

 

OTT TV BOX LINK: https://community.freescale.com/docs/DOC-94561

 

JB4.2 patches link : Patches for HDMI Dongle JB4.2.2_1.0.0-GA Release

Tags (2)
Attachments
Comments

We are designing this products, how to get your support?

Thank you very much, how can I get you and Mr.Jiang Wei's contact details?

Is the HDMI dongle available as a reference design?

Please contact our marking or sale guys.

Can you provide the contacts?

I contacted freescale sale support they said the only reference design were for the MCIMX6Q-SDP and MCIMX6Q-SDB eval boards.

This solution is completely made by chinese team.  You'd better ask the local sales ship from China.

I'd be interested in add support for it in Yocto; that's why I asked.

Someone I can contact to discuss it?

So far, we have no support for Yocto, but  unbuntu and android.   system is ready there.

How can we get uboot source and  ubuntu image?

There are two ways you can choose. you can use the last release you have and we can provide patch.

Another way is you can wait for the next release. The next release will have hdmi dongle support.

Do you know when next full release is planned for?

Also how can we get your contact details?

Should be soon in next month. You can call our sale to get the release plan.

For the contact detail, you can visit our support webpage and find the local sale.

Thanks for that. I've provided more instructions to build it in Ubuntu 12.04 64-bit in case some are interested.

http://www.cnx-software.com/2013/02/06/u-boot-linux-kernel-and-android-patches-for-freescale-i-mx6-h...

Great work! The schematics include additional circuity for LVDS, SATA etc, it doesn't look like the pcb layout include the io lines for theses? Furthermore what type of cooling heatsink would be the preferred option considering the small dimensions of the device.

Hi Jas, the NVCC_LVDS2P5 must be powered for this power is not only for LVDS display interface, but also for DDR I/O. This pin cannot be disconnected, even if the LVDS interface is not used. The SATA circuits are reserved for POWER ESATA interface which has not been used on revB2. As to the thermal design, aluminium is preferred for the heatsink.

It would be good if there was a TV box reference design with HDMI, USB, Ethernet and SATA.

The R13.4 GA release is no longer available and the patches don't seem to work with R13.4.1.  Is there another way to obtain the R13.4 GA Android source code?

Hello,

Is this board available now ?

I'd like to buy this mini PC for evaluation.

Thanks

M.Phuong

The board is available, you can ask fae to get it.

Dear Sir,

Sorry, what fae means ?

Could you please show me the contact ?

Regards

Hi Sir,

Sorry, you can not get the board for we do not sale the board, you can make the PCB by yourself.

please refer to link https://community.freescale.com/docs/DOC-94817 to get patches for JB4.2 hdmi dongle

Dear all,this is henry ,According to the freescales data ,we bulit  the PCBA samples ,if any body need this type samples ,pls contact with me .or you can leave some information .

[email protected]

How much cost each sample?

Cost 1~10 pcs     300USD/Unit

        11~50pcs    200USD/Unit

        51~100pcs   150USD/Uint

       >100pcs      Negotiate the Price .

For the first bacth had been sold out ,we begin the second bacth booking . And get the 50 pcs order total ,we will run the batch .

Hello Mr. Jiangwei,

Could you please provide the WM8326 config EEPROM data ?

Best Regards,

Thank you very much.

Hi ,

         I am having imx6q sabrelite board.

Is HDMI dongle android is same as normal android runs on imx6?

If want to make same thing on sabrelite board,What will be changes i need to do?

Thanks,

Pratik

Hi Pratik,

Is there a reason you're not using our (Boundary Devices') Android?

We fully support Android on the SABRE Lite platform:

The latest published binary release is '4.3-beta', but our source trees have been updated to include 4.3-ga.

     http://boundarydevices.com/second-release-jellybean-4-3-beta-mx6/

If you follow our blog, you'll see that we're documenting most of the steps we take:

     http://boundarydevices.com/tag/android/

Hi Eric,

     Thanks for fast reply, I am using imx6-jb-sdcard-20130628.img.gz on Board.

when I go through HDMI Dongle Design I Think to try same think out of sabrelite.

But you are saying Boundary Device's android is doing same thing as this dongle is doing , if I am right.

Will you please clarify that.

Thanks ,

Pratik.

Hi Pratik,

The image you listed is one of ours (a Boundary Devices' version), though a bit out-dated. Our latest Jellybean version is the second release pointed to above.

I haven't gone through the details, but I suspect the HDMI dongle release has the same origin, but has been tailored for different hardware.

Dear Wei:

   Dose you have config file of wm8326? Is it same with OTT  TV box?

Hi All:

hdmi dongle board can't bring up. When I use DDR_Stress_Tester_V1.0.2 to test the ddr, the board can't pass the DQS  gating, read/write delay calibration.  Pls see the log below:

What ARM core speed would you like to run?

Type 0 for 650MHz, 1 for 800MHz, 2 for 1GHz, 3 for 1.2GHz

  ARM set to 650MHz

Please select the DDR density per chip select (in bytes) on the board

Type 0 for 2GB; 1 for 1GB; 2 for 512MB; 3 for 256MB; 4 for 128MB; 5 for 64MB; 6

for 32MB

For maximum supported density (4GB), we can only access up to 3.75GB.  Type 9 to

select this

  DDR density selected (MB): 1024

Calibration will run at DDR frequency 528MHz. Type 'y' to continue.

If you want to run at other DDR frequency. Type 'n'

Enter the DDR frequency for calibration [350MHz to 528MHz]:

350

  The freq you entered was: 350

  DDR Freq: 352 MHz

Would you like to run the write leveling calibration? (y/n)

  Please enter the MR1 value on the initilization script

  This will be re-programmed into MR1 after write leveling calibration

  Enter as a 4-digit HEX value, example 0004, then hit enter

0004 You have entered: 0x0004

Start write leveling calibration

Write leveling calibration completed

MMDC_MPWLDECTRL0 ch0 after write level cal: 0x00010001

MMDC_MPWLDECTRL1 ch0 after write level cal: 0x00180018

MMDC_MPWLDECTRL0 ch1 after write level cal: 0x000A0013

MMDC_MPWLDECTRL1 ch1 after write level cal: 0x000A0015

Would you like to run the DQS gating, read/write delay calibration? (y/n)

Starting DQS gating calibration...

. . . . . . . . . . . . . . ERROR FOUND, we can't get suitable value !!!!

dram test fails for all values.

The DDR stress test can run with an incrementing frequency or at a static freq

To run at a static freq, simply set the start freq and end freq to the same valu

e

Would you like to run the DDR Stress Test (y/n)?

End of Test !

^C

D:\DDR_Stress_Tester_V1.0.2\DDR_Stress_Tester_V1.0.2\Binary>

When I use MFG tools of OTT TV box, It stopped at Loading uboot

Inline image 2

So, What's wrong? DDR is not ok?

No ratings
Version history
Last update:
‎11-22-2012 06:41 PM
Updated by: