Flutter SDK installation for Linux Desktop Image on the i.MX8MP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flutter SDK installation for Linux Desktop Image on the i.MX8MP

Flutter SDK installation for Linux Desktop Image on the i.MX8MP

On this tutorial we will review the implementation of Flutter on the i.MX8MP using the Linux Desktop Image.

スポイラ
Please find more information about Flutter using the following link: Flutter: Option to create GUIs for Embedded System... - NXP Community

Requirements:

Evaluation Kit for the i.MX 8M Plus Applications Processor. (i.MX 8M Plus Evaluation Kit | NXP Semiconductors)

NXP Desktop Image for i.MX 8M Plus (GitHub - nxp-imx/meta-nxp-desktop at lf-6.1.1-1.0.0-langdale)

Note: This tutorial is based on the NXP Desktop Image with Yocto version 6.1.1 – Langdale.

Steps:

1. First, run commands to update packages.

$ sudo apt update
$ sudo apt upgrade

2. Install Flutter for Linux using the following command.

$ sudo snap install flutter --classic

3. Run the command to verify the correct installation.

$ flutter doctor

With this command you will find information about the installation. The important part for our purpose is the parameter "Linux toolchain - develop for Linux desktop".

4.png

4. Run the command “flutter create .” to create a flutter project, this framework will create different folders and files used to develop the application. 

$ cd Documents
$ mkdir flutter_hello
$ cd flutter_hello
$ flutter create .​

5.png

5. Finally, you can run the “hello world” application using:

$ flutter run

6.png7.png

Verify the program behavior incrementing the number displayed on the window.

 

100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎07-25-2024 12:00 PM
更新者: